Hi,
I am working on P2020 QoriIQ.
Is there a way to know which of the Interrupt Vector Registers (IVOR0 - IVOR35) accured?
I`m searching for register that will tell me the IVOR number in my exceptions handler.
Thanks for help :smileyhappy:
The Table 9-2 of the P2020 Reference Manual contains the assignments of the internal interrupt.
Linux makes no difference between external and internal interrupts. All interrupts in the system are handled by the same Linux API. If this API didn't work, no driver in the system would be able to operate, not just your customer's module.
The customer is attempting to request an IRQ by the resource number which is generally incorrect. The resource number is an index to irq_desc table.
This index is generally _not_equal to the hardware IRQ line number. See Documentation/IRQ.txt for explanation.
To request an IRQ line in a proper way, the customer should:
property is calculated by the following
formula:
[DTS_interrupt_number] = ([EIVPR/IIVPR_addr] - [Interrupt_Source_Configuration_Registers_Base]) / 0x20
where [EIVPR/IIVPR_addr] is the address of the interrupt configuration registers
of the IRQ being declared, [Interrupt_Source_Configuration_Registers_Base]
is 0x50000 for P2020
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------