Hi there,
I currently have a LS1012A Reference Design Board, with OpenWRT vls1012a.ear1.rc2.
When I do "opkg update", it comes out the error "opkg_download: Failed to download http://downloads.openwrt.org/chaos_calmer/15.05/ls1012a/hgw/packages/base/Packages.gz, wget returned 1."
Looking at OpenWRT there doesn't seem to have support for ls1012a.
How does one update/upgrade with opkg for this reference board? Should I be pointing to download Packages.gz to somewhere else?
Thanks.
Yes, there is no "ls1012a" in downloads.openwrt.org/chaos_calmer/15.05
To get an access to new software releases of ASK software for LS1012A, you need support plan.
Please look the following page for more details:
QorIQ LS1012A, LS1024A and LS102MA Processor Suppo|NXP
Have a great day,
Alexander
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Is there any workaround for this?
I have a week to evaluate this board along with other NXP processors to see if it fits our specs. If we're not able to get certain packages/features then it would be difficult to fully evaluate this processor.
Thanks,
Acer