NCSW files for P1020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NCSW files for P1020

578 次查看
jm1015
Contributor II

Hello,

   On building NCSW code for P1020 using GHS Multi,.

The compiler is not able to locate "types_ghs.h" file. This causes undeclared error for uintptr_t, int64_t, int32_max etc. 

Does this file comes with NCSW package or GHS multi or its user defined ??

0 项奖励
1 回复

469 次查看
alexander_yakov
NXP Employee
NXP Employee

I see "types_ghs.h" is included only in case if __GHS__ is defined, that means this file is specific to GHS. I do not see this file included in NCSW package, so I think it should be a part of GHS.

Note we do not have experience too much compiling NCSW with GHS, so I recommend using our CodeWarrior compiler to compile this package.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励