Mode Registers!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mode Registers!

702件の閲覧回数
qammarabbas
Contributor IV

Hi,

While configuring the registers of T1042 for the DDR memory controller, i encountered a field "UNQ_MRS_EN" in the DDR_DDR_SDRAM_CFG_2 register and i am unable to comprehend what does it mean. Can anybody please explain what is it for and when to use it?

タグ(1)
0 件の賞賛
4 返答(返信)

574件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ T1040 Reference Manual, 14.4 DDR Memory Map/Register Definition.

If DDR_DDR_SDRAM_CFG_2[UNQ_MRS_EN]=0 then for all chip selects data from the following MODE registers will be used:

DDR_DDR_SDRAM_MODE

DDR_DDR_SDRAM_MODE_2

DDR_DDR_SDRAM_MODE_9

DDR_DDR_SDRAM_MODE_10

If DDR_DDR_SDRAM_CFG_2[UNQ_MRS_EN]=1 then individual data from the following MODE registers will be used:

for CS0:

DDR_DDR_SDRAM_MODE

DDR_DDR_SDRAM_MODE_2

DDR_DDR_SDRAM_MODE_9

DDR_DDR_SDRAM_MODE_10

for CS1:

DDR_DDR_SDRAM_MODE_3

DDR_DDR_SDRAM_MODE_4

DDR_DDR_SDRAM_MODE_11

DDR_DDR_SDRAM_MODE_12

for CS2:

DDR_DDR_SDRAM_MODE_5

DDR_DDR_SDRAM_MODE_6

DDR_DDR_SDRAM_MODE_13

DDR_DDR_SDRAM_MODE_14

for CS3:

DDR_DDR_SDRAM_MODE_7

DDR_DDR_SDRAM_MODE_8

DDR_DDR_SDRAM_MODE_15

DDR_DDR_SDRAM_MODE_16

0 件の賞賛

574件の閲覧回数
qammarabbas
Contributor IV

Could you please elaborate when to enable this bit and when to clear? Thank you!

0 件の賞賛

574件の閲覧回数
ufedor
NXP Employee
NXP Employee

It is up to the board designer.

0 件の賞賛

574件の閲覧回数
qammarabbas
Contributor IV

what information does the board designer need to know before setting/clearing this bit?

0 件の賞賛