MPC5200Cxx400 REV.2 availability or use REV.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5200Cxx400 REV.2 availability or use REV.4

320 次查看
peterjuul
Contributor I

Is MPC5200CVR400 or MPC5200CBV400 REV.2 available and if so, how can it be ordered ? 

What is changed from REV.2 to REV.4 ?  

Will a circuit (including software) designed for a REV.2 chip ALLWAYS work if updating to a REV.4 chip ?

0 项奖励
1 回复

255 次查看
Pavel
NXP Employee
NXP Employee

The MPC5200Cxx400 is the MPC5200 Rev A.

The MPC5200CVR400 is the MPC5200 Rev A in 272 TE-BGA packages.

The MPC5200CBV400 is the MPC5200 Rev A in 272 TE-BGA Pb-free packages.

All circuit and all software work on the MPC5200Cxx400 Rev 2 and Rev 4.

The MPC5200Cxx400B is the MPC5200 Rev B. Look at the AN3045 about difference between Rev A and Rev B:

http://www.nxp.com/assets/documents/data/en/application-notes/AN3045.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励