Linux SDK & P4080PCIe EVA board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux SDK & P4080PCIe EVA board

1,586 Views
alexanderlange
Contributor I

Hello,

can anybody explain, what kind of changes to the Linux SDK (V1.4) have to be done to get the P4080PCIe EVA board running.

When using the P4080DS configuration the kernel is booting but seems to fail during ethernet driver setup.

I used the original U-Boot (2010.12) to download the images.

0 Kudos
7 Replies

1,169 Views
yipingwang
NXP TechSupport
NXP TechSupport


Please refer to a SDK 1.0 based patch tar ball P4080-PCIE-SDK-1.0-05-03-2012.tgz from Run-time Software in http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=P4080PCIE&nodeId=018rH325E40180&fpsp=....

0 Kudos

1,169 Views
scottwood
NXP Employee
NXP Employee

Does that 1.0 SDK have all the current errata workarounds?

0 Kudos

1,169 Views
alexanderlange
Contributor I

Thanks for reply. Unfortunately this patch seems only to work with version 1.0 and can not be executed in the 1.4 environment.

0 Kudos

1,169 Views
lunminliang
NXP Employee
NXP Employee

Why not using the one as Yiping indicated? Is there any special requirement?

0 Kudos

1,169 Views
JohnOldfield
Contributor II

Finding this thread later, I can only find the current 2.3 release (QorIQSDK_02_03_00B_ltib.iso). It appears that the current 2.3 release has changed significantly and doesn't appear to support the P4080PCIe card.

How do I find the QorIQ-DPAA-SDK-20110609-systembuilder.iso file that the above release notes refer to?

0 Kudos

1,169 Views
scottwood
NXP Employee
NXP Employee

2.3B is not the current SDK -- it is a beta version that is older than 1.0.  The latest SDK release is 1.4.  1.4 supports p4080, but you may need to migrate board code yourself.

0 Kudos