[LS1043ARDB] no pinctrl handle

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[LS1043ARDB] no pinctrl handle

3,770 Views
randy_wang
Contributor II

Hi,

I modprobe TPM driver: tpm_tis_spi.

but get the error message:

no pinctrl.PNG

and I modified the device tree file ls1043a-rdb.dts for dspi  as following:

......

&dspi0 {
bus-num = <1>;
status = "okay";

flash@0 {
#address-cells = <1>;
#size-cells = <1>;
compatible = "n25q128a13", "jedec,spi-nor"; // 16MB /
reg = <0>;
spi-max-frequency = <1000000>; // input clock /
};

tcg@1 {
compatible = "tcg,tpm_tis-spi";
reg = <1>;
#address-cells = <1>;
#size-cells = <0>;
spi-max-frequency = <500000>;
pinctrl-names = "default";

};

...

Please help.

Thanks,

Randy

Tags (1)
0 Kudos
Reply
3 Replies

3,373 Views
Pavel
NXP Employee
NXP Employee

Do you use the following in LSDK 18.09 kernel menu for TPM enabling:

Device Drivers  --->

                  Character devices  ---> 

                               <*> TPM Hardware Support  --->

                                               TPM Interface Specification 1.3 Interface / TPM 2.0 FIFO Interface - (SPI) 


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,373 Views
randy_wang
Contributor II

Hi Pavel,

Thanks for your reply.

Yes, I have set the TPM enabled in LSDK1803 kernel menu.

As the dmesg shows, and I had traced the tpm_tis_spi driver code.

found that I cannot get the response as TPM_ACCESS_VALID(0x80) form TPM.

I just got 0x00 response, and got 0xff response when the TPM unplugged.

Should I do any settings about the dspi/spi ?

Thanks.

Randy 

0 Kudos
Reply

3,373 Views
randy_wang
Contributor II

I have solve this issue.

And port the Infineon TPM on LS1043 successfully.

the key points is:

TPM SPI driver encapsulates the first 4 bytes as a single message, and try to read status byte from another message, so it try to keep CS as assertion by setting cs_change to 1.

However, the NXP SPI driver will not set its dspi->cs_change value according the cs_change of transfer object passed by TPM SPI driver

Thanks.

0 Kudos
Reply