Hi experts,
we have a custom board on this board we will have to perform production test SW. For this application we will have to use a simple application (like baremetal) running on OCRAM that execute some device tests present on the board.
I use codeWarrior IDE but missing the SDK/libraries, in this moment I have run the hello word demo from OCRAM and I am started with Processor Expert to configure our DDR4 controller (now working yet).
We want to test I2c, SPI and a couple of UARTs.
Where can I find the SDK for this scope?
Thak you for your suypport.
Best Regards.
Dario
Dario, are you looking for something to load from ocram only ? (I think the the link above for baremetal app requires to boot u-boot first off the sd or flash then loads and runs the test app on the ram)
Regards
Sinan Akman
Hi,
the use od OCRAM is not important now (we have solved DDR3 memory problem), but we need to use a bare metal application, we can't use uboot or orhers.
I hope to can supprt us in this.
Best Regards,
Dario
There is no complete baremetal solution from NXP.
You could create a bare metal project in CodeWarrior IDE, then refer to u-boot to develop baremetal driver by yourself.
You could refer to "3.2.4 Development based on BareMetal framework" in https://www.nxp.com.cn/docs/en/user-guide/REALTIMEEDGEUG_REV2.2.pdf.