LS1043A Security Engine (SEC) Job Ring Initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1043A Security Engine (SEC) Job Ring Initialization

413 Views
rjschirmer
Contributor I

I'm am trying to reset/initialize the SEC Job Rings.  Here is the pseudo-code of what I am doing to reset a SEC Job Ring Controller:

writeReg32(JRCFGR_JRx_LS[IMSK], 1)   // Mask interrupts
writeReg32(JRCR_JRx, RESET, 1)   // Initiate a flush
while( readReg32(JRINTR_JRx, HALT) == 1 )  // While halt in progress
return Error if (readReg32(JRINTR_JRx, HALT) != 2) // Return error if halt not complete
writeReg32(JRCR_JRx, RESET, 1)   // Initiate a reset (after flush)
while( readReg32(JRCR_JRx, RESET) != 0 ) // Wait for reset to complete
writeReg32(JRCFGR_JRx_LS[IMSK], 0)   // Unmask interrupts
return Success

However the "halt in progress" (on the third line) is never deasserted.  And if I skip over the above initialization then the BSY bit is stuck set in the SSTA register and if I enable interrupts on Job Ring 1 then the interrupt is always asserted with a  I keep getting interrupts on Job Ring 1 with a value 0x03030000 in interrupt status register JRINTR_JR0 (i.e. no status asserted).

I have two questions:

1) Is the above pseudo-code showing the correct method for resetting the Job Ring Controller?

2) Is there anything else I should be doing to reset or initialize the Job Ring Controllers?

0 Kudos
Reply
3 Replies

325 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please ask customer refer to reference code in u-boot
uboot/drivers/crypto/fsl/jobdesc.c, jr_hw_reset()

0 Kudos
Reply

316 Views
rjschirmer
Contributor I
Where is the recommended repository where I can find this u-boot code?
0 Kudos
Reply

347 Views
yipingwang
NXP TechSupport
NXP TechSupport

Discussing with the SE team.

0 Kudos
Reply