LS1043A Debug port in UART

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1043A Debug port in UART

540件の閲覧回数
logeshs
Contributor II

Hi,

We are    LS1043A in our design, can you please confirm shall we use UART2 as the Debug port? we have connected UART1 with Network Switch.

Thanks

0 件の賞賛
2 返答(返信)

388件の閲覧回数
Pavel
NXP Employee
NXP Employee

Look at the Section 2.3.1 of the LS1043ARDB Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1043ARDBRM&Parent_nodeId=1441121579998719223109&Parent...

 

This Section contains instruction for using UART2 as terminal.

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

388件の閲覧回数
logeshs
Contributor II

Thanks for your reply. So we can use any of the UART port as Debug terminal. 

Also in the Debug port we are using CTS and RTS pins and UART which connected to Switch does not use CTS and RTS.  If that is the case i hope we shall not configure the CTS and RTS of UART  which is connected to Switch as GPIO. Please confirm my understanding.

0 件の賞賛