Hi,
We are developing a custom board that will have only 128Mbytes DDR3L RAM memory. We got the board booting uboot but when booting linux it is not working. The clock we are using is a 100MHz differential clock.
I just took the tower dev kit, removed the resistors frm the clocking circuit so that the config matches my board. In the RCW I config the DDR3 clock to use the differential one and I am able to boot from the SD card After this I just tried booting linux modifying the mem parameter in the kernel command line and as soon as I use a value lower than 512M the kernel stops booting.
Is there any minimum requierement for booting linux in this platform?
Thanks,
Daniel,
解決済! 解決策の投稿を見る。
OK, I was able to answer myself.
Both uboot and the dts file for the board must have the same value in the memory size configuration:
In uboot :
#define PHYS_SDRAM_SIZE | (128u * 1024 * 1024) |
In the dts file:
memory@80000000 {
device_type = "memory";
reg = <0x0 0x80000000 0x0 0x8000000>;
};
OK, I was able to answer myself.
Both uboot and the dts file for the board must have the same value in the memory size configuration:
In uboot :
#define PHYS_SDRAM_SIZE | (128u * 1024 * 1024) |
In the dts file:
memory@80000000 {
device_type = "memory";
reg = <0x0 0x80000000 0x0 0x8000000>;
};