LS1021A-TWR flex-builder fails with mkfw instruction

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1021A-TWR flex-builder fails with mkfw instruction

545件の閲覧回数
nenadradulovic
Contributor I

SDK: LayerScape version LSDK-17.09

When invoking flex-builder with:

flex-builder -i mkfw -b sd -B uboot -m ls1021atwr

it fails with the following message:

dd: failed to open 'build/firmware/qe-ucode/fsl_qe_ucode_1021_10_A.bin': No such file or directory

This file is specified in file: manifest/ls1021atwr.manifest.

Quick scan through scripts in tools/ folder shows that there is no mechanism to transfer mentioned file into the path.

Also, Makefile located in packages/firmware folder creates invalid link to file flexbuild/packages/firmware/qe-ucode which does not exists.

Workaround: manually copy the file there.

0 件の賞賛
1 返信

374件の閲覧回数
nenadradulovic
Contributor I

Ok, this was my mistake. Once I moved the root folder location the links in buoild/images got invalidated. The Makefile otherwise creates valid links.

0 件の賞賛