LS1021A IFC_TA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1021A IFC_TA

Jump to solution
2,893 Views
henrybausley
Contributor I

We now have a prototype LS1021 board running and I have one unsolved problem.

I am using IFC_CS1 to access our FPGA and everything works except the transfer acknowledge (IFC_RB1_B).

I have verified that the signal is going low for two IFC_CLK cycles but the access does not stop until it times out.

I have change the timeout time to verify that this is what is happening.

If I disable the transfer acknowledge the timing works as described in the manual.

The IFC_CS1 is in the normal GPCM operation mode.

The one thing in the manual that concerns me is that IFC_RB1_B is a dual function pin with SPI1_SIN as the other option.

There is nothing in the manual that tells what controls this pins function.

0 Kudos
1 Solution
2,399 Views
ufedor
NXP Employee
NXP Employee

Got this confirmation from design about pin muxing this morning.

RCW[405]---Together with IFC_GRP_E1_EXT_FIELD, this field configures the functionality of group E1 of the IFC pins: IFC_CS[1:3]_B and IFC_RB[1]_B

0: IFC_CS[1:3]_B, IFC_RB[1]_B

1: GPIO2[10:12], Reserved

RCW[396:398]---This group configures the functionality of group E1 of the IFC pins together with IFC_GRP_E1_BASE field:IFC_CS[1:3]_B,IFC_RB[1]_B

000:IFC_GRP_E1_BASE field definition

001: SPI1_PCS0, SPI1_SCK,QSPI_DIO3_B, SPI1_SIN

010: FTM7_CH0, FTM_CH1, FTM7_EXTCLK, Reserved

100: IFC_CS1_B, IIC3_SCL, IIC3_SDA, Reserved

Your RCW shows that [396:398]=100 - i.e.:

100: IFC_CS1_B, IIC3_SCL, IIC3_SDA, Reserved

Please set it to 000 and set RCW[405]=0.

View solution in original post

0 Kudos
6 Replies
2,400 Views
ufedor
NXP Employee
NXP Employee

Please send the IFC registers dumps when IFCTA is set to terminate transaction, before and after IFC_RB1 is asserted by FPGA.

Please provide scope shot of IFC_RB1 at FPGA and SoC boundary and schematic of IFC (to check pull up for IFC_RB1).

0 Kudos
2,400 Views
henrybausley
Contributor I

When using CS2 and IFC_RB0 we can get the expected results so we know our CPLD logic is correct.  CS1 and IFC_RB1 does not seem to work for us.  Is it possible  IFC_RB1 is setup in an alternate configuration SPI1_SIN?

0 Kudos
2,400 Views
ufedor
NXP Employee
NXP Employee

Got this confirmation from design about pin muxing this morning.

RCW[405]---Together with IFC_GRP_E1_EXT_FIELD, this field configures the functionality of group E1 of the IFC pins: IFC_CS[1:3]_B and IFC_RB[1]_B

0: IFC_CS[1:3]_B, IFC_RB[1]_B

1: GPIO2[10:12], Reserved

RCW[396:398]---This group configures the functionality of group E1 of the IFC pins together with IFC_GRP_E1_BASE field:IFC_CS[1:3]_B,IFC_RB[1]_B

000:IFC_GRP_E1_BASE field definition

001: SPI1_PCS0, SPI1_SCK,QSPI_DIO3_B, SPI1_SIN

010: FTM7_CH0, FTM_CH1, FTM7_EXTCLK, Reserved

100: IFC_CS1_B, IIC3_SCL, IIC3_SDA, Reserved

Your RCW shows that [396:398]=100 - i.e.:

100: IFC_CS1_B, IIC3_SCL, IIC3_SDA, Reserved

Please set it to 000 and set RCW[405]=0.

0 Kudos
2,400 Views
henrybausley
Contributor I

Attached is a PDF of the CPU to CPLD connection.

If we force RB0 to low IFC_RB_STAT indicates RB0,RB2.RB3,RB4,RB5,RB6 change state.

If we force RB1 there is no change in the IFC_RB_STAT register.

Normal Mode:

Chip select is green Chanel 4,  RB1 is blue Chanel 3

APM1.jpg

This is with termination and you can see it times out

APM2.jpg

We tried inverting RB1 for a test of the status bit

APM3.jpg

0 Kudos
2,400 Views
ufedor
NXP Employee
NXP Employee

Which RCW is used?

What are IFC CS1 settings?

0 Kudos
2,400 Views
henrybausley
Contributor I

CPU:   Freescale LayerScape LS1021, Version: 2.0, (0x87001120)

Clock Configuration:

       CPU0(ARMV7):1000 MHz,

       Bus:300  MHz, DDR:800  MHz (1600 MT/s data rate),

Reset Configuration Word (RCW):

       00000000: 0608000a 00000000 00000000 00000000

       00000010: 20000000 00403900 e0025a00 21046000

       00000020: 00000000 00000000 00000000 18000000

       00000030: 00080000 481b7340 00000000 00000000

From file*******************************************************************

#define CONFIG_SYS_CPLD_BASE 0x7f000000

#define CPLD_BASE_PHYS CONFIG_SYS_CPLD_BASE

#define CONFIG_SYS_FPGA_CSPR_EXT        (0x0)

#define CONFIG_SYS_FPGA_CSPR (CSPR_PHYS_ADDR(CPLD_BASE_PHYS) | \

  CSPR_PORT_SIZE_16 | \

  CSPR_MSEL_GPCM | \

  CSPR_V)

#define CONFIG_SYS_FPGA_AMASK IFC_AMASK(16 * 1024 * 1024)

#define CONFIG_SYS_FPGA_CSOR (CSOR_GPCM_GPMODE_NORMAL | \

  CSOR_GPCM_GPTO(256) | \

  CSOR_GPCM_RGETA_EXT | \

  CSOR_GPCM_WGETA_EXT | \

  CSOR_GPCM_ADM_SHIFT(4) | \

  CSOR_GPCM_BURST(2) | \

  CSOR_GPCM_TRHZ_20 | \

  CSOR_GPCM_BCTLD)

#define CONFIG_SYS_FPGA_FTIM0 (FTIM0_GPCM_TACSE(0x1) | \

  FTIM0_GPCM_TEADC(0x01) | \

  FTIM0_GPCM_TEAHC(0x01))

#define CONFIG_SYS_FPGA_FTIM1 (FTIM1_GPCM_TACO(0x01) | \

  FTIM1_GPCM_TRAD(0x21))

#define CONFIG_SYS_FPGA_FTIM2 (FTIM2_GPCM_TCS(0x1) | \

  FTIM2_GPCM_TCH(0x1) | \

  FTIM2_GPCM_TWP(0x21))

#define CONFIG_SYS_FPGA_FTIM3           FTIM3_GPCM_TAAD(0x06)

From memory big endian******************************************************

IFC_CSPR1(0x153001c) = 0x7f000105

IFC_AMASK1(0x15300ac) = 0xff000000

IFC_CSOR1_GPCM(0x153013c) = 0x000c8201

IFC_FTIM0_CS1_GPCM(0x15301f0) = 0x10010001

IFC_FTIM1_CS1_GPCM(0x15301f4) = 0x01002100

IFC_FTIM2_CS1_GPCM(0x15301f8) = 0x01040021

IFC_FTIM3_CS1_GPCM(0x15301fc) = 0x18000000

0 Kudos