Hi All,
I've gotten a LS1012a RDB and I'm Trying to learn to use it.
The problem I have is the drive doesn't appear when it is plugged in, and only appeared as a drive called BOOTLOADER once I clicked the reset button.
Could anyone help me get the board connected?
I'm sorry is this question has been asked before, but any help is greatly appreciated.
Many thanks in advance,
Nic
Sorry for the delay,
Yes I have followed the guide, but when I plug in the USB the PC doesn't install USB drivers and the serial port driver can't be installed.
additionally there are no com ports listed and Tera Term can't start a serial connection.