LS1012A SerDes spread-spectrum clock source recommendations

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1012A SerDes spread-spectrum clock source recommendations

425 Views
MugaNathan
Contributor I

In LS1012A I need to use both the PCIe & SGMII(100Mbps speed) interface simultaneously for data transfer, will this SerDes spread-spectrum clocking support both simultaneously or any one at a time.

0 Kudos
Reply
1 Reply

404 Views
yipingwang
NXP TechSupport
NXP TechSupport

Spread-spectrum clocking cannot be used if the same SerDes reference clock is shared with other non-spread-spectrum-supported protocols. For example, if spread-spectrum clocking is desired on a SerDes reference clock for the PCI Express protocol and the same reference clock is used for any other protocol, such as SATA or SGMII because of the SerDes lane usage mapping option, spread-spectrum clocking cannot be used at all.

0 Kudos
Reply