Hi,
MPC8572_E cpu is a dual core, we are using one core loaded with ios image and second core was brought up with Linux 2.6.32. we are looking for options to enable KVM on the dual core,
by editing /nobackup/usr1/sup2t/target/configs/p1021_c800_kernel_defconfig
and adding vt and kvm config
CONFIG_VIRTUALIZATION=y
CONFIG_KVM=y
CONFIG_KVM_E500=y
CONFIG_TUN=y
and while building kernel image, following error message was displayed. "error: too many arguments to function 'trace_kvm_stlb_inval'"
please do the needful in helping to build kernel image with KVM support.
Error message:
bgl-ads-1348:240> make CWAN_PLATFORM=p1021_c800
Creating rootfs structure
Creating target root file
system...
----------- compile =>
/nobackup/usr1/sup2t/hostTools/tools -----------
----------- compile =>
/nobackup/usr1/sup2t/u-boot -----------
----------- compile =>
/nobackup/usr1/sup2t/kernel-2.6.32 -----------
make: ***
[compile_!nobackup!usr1!sup2t!kernel-2.6.32] Error 2
bgl-ads-1348:241>
Logs in buildlogs:
arch/powerpc/kvm/e500_tlb.c: In
function 'kvmppc_e500_stlbe_invalidate':
arch/powerpc/kvm/e500_tlb.c:229:
error: too many arguments to function 'trace_kvm_stlb_inval'
make[3]: ***
[arch/powerpc/kvm/e500_tlb.o] Error 1
make[2]: *** [arch/powerpc/kvm]
Error 2
make[2]: Leaving directory
`/nobackup/usr1/sup2t/kernel-2.6.32/linux-2.6.32'
make[1]: *** [compile] Error 2
make[1]: Leaving directory
`/nobackup/usr1/sup2t/kernel-2.6.32'
bgl-ads-1348:230>
Thanks
Manikantag
已解决! 转到解答。
1. Which Freescale Linux BSP you are using?
2. Why "P1021" is mentioned here, if the device is MPC8572 ?
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
1. Which Freescale Linux BSP you are using?
2. Why "P1021" is mentioned here, if the device is MPC8572 ?
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
MPC8572 is a dual core, in one core running ios image and we brought up second core with Linux image 2.6.32, this image was given by freescale team to boot up second core with Linux. P1021 is the image type used to turn on dual core, boot kernel and Linux OS.
p1021_c800-uboot-image.bin
rootfs_p1021_c800.ext2.gz.uboot
p1021_c800-linux-image.uImage
thanks
Manikantag
Hi,
Was able to find solution to this issue,
http://comments.gmane.org/gmane.comp.emulators.kvm.devel/53613
Now I am trying to bringup VT and KVM on it, is there any procedures to be followed to make it up. please share the info for the same.
Thanks
Manikantag