Is is possible to reconfigure SerDes in T2080?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is is possible to reconfigure SerDes in T2080?

1,156 次查看
gregbuchannan
Contributor I

My RCW configures two SerDes lanes as XFI.  I would like to reconfigure these lanes as SGMII or 1000Base-X.  Is it possible to do this via reconfiguration of the SerDes control registers?

0 项奖励
7 回复数

910 次查看
gregbuchannan
Contributor I

For example, table 19-1 has no SRDS1: A/SG9 - B/SG10 - C/XFI1 - D/XFI2 (I don't care about E,F,G,H).   Going through the SerDes register settings, this looks like it could be configured as long as I use PLL1 for lanes 0/1 and PLL2 for lanes 2/3.    (I know there is a XFI/XFI/SG/SG configuration in the table, but I am trying to support my current board connections.)

0 项奖励

910 次查看
ufedor
NXP Employee
NXP Employee

> SRDS1: A/SG9 - B/SG10 - C/XFI1 - D/XFI2

This configuration is not possible because XFI lanes always use PLL1 and lanes A & B also always use PLL1.

0 项奖励

910 次查看
gregbuchannan
Contributor I

Looking at the descriptions for the Serdes General Control Register 0 SerDesx_LNnGCR0,  I see that lanes A & B must use PLL1, but that I can also set lanes C - H to use PLL2.  I can't find any SerDes register description that requires XFI to use PLL1 (other than the RCW table).  Is this limitation documented somewhere?  I may be missing it.  Thanks.

0 项奖励

910 次查看
ufedor
NXP Employee
NXP Employee

Response from the Applications Team:

"We don't have this option in RM and they cannot use this combination. We only support the options published in RM."

0 项奖励

910 次查看
gregbuchannan
Contributor I

Section 19.6 of the RM, particularly Section19.6.4, indicate that the SerDes can be reconfigured after POR RCW configuration by writing to the appropriate SerDes registers (assuming the necessary RefClk and PLL frequencies are available).  I am misinterpreting this section?

0 项奖励

910 次查看
ufedor
NXP Employee
NXP Employee

Which SerDes protocol pair is in question?

0 项奖励

910 次查看
ufedor
NXP Employee
NXP Employee

All supported SerDes configurations are shown in the T2080RM, Table 19-1. SerDes Lanes Assignments and Multiplexing.

Other configurations are not supported.

0 项奖励