We see that PPC_DISABLE_THREADS only needed for e6500 Rev1 chip; However we see that, if we dont use this even for our Rev2 processor core, then we see that CPU get stuck in high traffic condition when the traffic is stopped after few hours; When we enable this erratum, only then, the issue goes away. however only 12 cores can be used now.
I need to know, whether this change is required for Rev2?
If we do the change, are there any side effects because we, now, get only 12 cores instead of 24 cores?
Share the errata please?
It is not obvious which hardware erratrum (or errata) is causing the issue, so additional investigation is needed.
> What more info you need for technical case than this?
Please provide a technical explanation of the issue reproducibility.
> Hiw do we create it?
Please refer to the link in the first response.