Hi,
I am currently working on ls1043ardb board.In the reference board the ppa is fetched from NOR location(60500000) by default(for all boot modes). I am trying to change the ppa address for nand that is ,if i am booting from nand it should take ppa from nand itself.
I have modified the following files:
1=>include/configs/ls1043ardb.h
2=>arch/arm/cpu/armv8/fsl-lsh2/ppa.c
The modifications are given below:
1=>
#ifdef CONFIG_NAND_BOOT
#define CONFIG_SYS_LS_PPA_FW_IN_NAND
#ifdef CONFIG_SYS_LS_PPA_FW_IN_NAND
#define CONFIG_SYS_QE_FW_IN_NAND
#define CONFIG_SYS_LS_PPA_FW_ADDR 0x220000
#endif
#else
#define CONFIG_SYS_LS_PPA_FW_IN_NOR
#ifdef CONFIG_SYS_LS_PPA_FW_IN_NOR
#define CONFIG_SYS_LS_PPA_FW_ADDR 0x60500000
#endif
The above modifications are in file1.
2=>
#if defined(CONFIG_SYS_LS_PPA_FW_IN_NOR)
fit_hdr = (void *)CONFIG_SYS_LS_PPA_FW_ADDR;
printf("\nHEader1:%p",fit_hdr);
#elif defined(CONFIG_SYS_LS_PPA_FW_IN_NAND)
fit_hdr = (void *)CONFIG_SYS_LS_PPA_FW_ADDR;
printf("\nHeader:%p",fit_hdr);
#else
#error "No CONFIG_SYS_LS_PPA_FW_IN_xxx defined"
#endif
These modifications are in ppa.c
But still i am getting the below given issue:
fsl-ppa: Bad firmware image (not a FIT image)
fsl-ppa: error (-22)
tzc380_init: add 0 regions
tzc380: tzc380_reg_base = 0000000001500000
Whats the issue?Is there any other modifications needed apart from this??
Pls help
Thanks in advance
Look at the following page:
and
https://patchwork.ozlabs.org/patch/569954/
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The LS1043 SDK 0.5 provides loading of the Primary Protected Application (PPA) image using NOR Flash only. Find the following in the ppa.c file:
#ifdef CONFIG_SYS_LS_PPA_FW_IN_NOR
fit_hdr = (void *)CONFIG_SYS_LS_PPA_FW_ADDR;
#else
#error "No CONFIG_SYS_LS_PPA_FW_IN_xxx defined"
#endif
See the following pages:
http://lists.denx.de/pipermail/u-boot/2016-February/246260.html
and
https://patchwork.ozlabs.org/patch/569954/
and
https://www.mail-archive.com/search?l=u-boot@lists.denx.de&q=subject:%22Re%5C%3A+%5C%5BU%5C-Boot%5C%...//www.mail-archive.com/search?l=u-boot@lists.denx.de&q=subject:%22Re%5C%3A+%5C%5BU%5C-Boot%5C%5D+%5C%5BPATCH+2%5C%2F3%5C%5D+ARMv8%5C%2Flayerscape%5C%3A+Add+FSL+PPA+support%22&o=newest&f=1
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pavel,
Is there any way to change the ppa.c so as to fetch ppa from NAND???
I have done the following modifications in ppa.c:
if defined(CONFIG_SYS_LS_PPA_FW_IN_NAND)
nand_info_t nand_info[CONFIG_SYS_MAX_NAND_DEVICE];
size_t fw_length = CONFIG_SYS_QE_FMAN_FW_LENGTH;
void *fit_hdr = malloc(CONFIG_SYS_QE_FMAN_FW_LENGTH);
rc = nand_read(&nand_info[0], (loff_t)CONFIG_SYS_LS_PPA_FW_ADDR,
&fw_length, (u_char *)fit_hdr);
if (rc == -EUCLEAN) {
printf("NAND read of PPA at offset 0x%x failed %d\n",
CONFIG_SYS_LS_PPA_FW_ADDR, rc);
}
But it seems like it does not work.Is there any other way to do it?
Pls help