How to use the multiplexed configuration pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the multiplexed configuration pins

730 Views
nishad_kamdar
Contributor IV

As mentioned in the P1022RM, the configuration pins are multiplexed with some of the bidirectional pins.

In case one of interfaces connected to these pins needs a pull up resistor, for instance (WE# of the NAND Flash (LFALE)) and I need to input a 0 to the config pin of the processor for a particular configuration, how can I achieve this (without an FPGA or a CPLD) as I cannot connect a pull up and a pull down on the same pin/connection.

0 Kudos
Reply
1 Reply

598 Views
lunminliang
NXP Employee
NXP Employee

See below technical support comment:

All configuration signals (including LFALE) have to be pulled to the desired values (either high or low) during POR.After POR the POR configuration signals are pure outputs and, thus, are actively driven.

0 Kudos
Reply