How to use the multiplexed configuration pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use the multiplexed configuration pins

675 Views
nishad_kamdar
Contributor IV

As mentioned in the P1022RM, the configuration pins are multiplexed with some of the bidirectional pins.

In case one of interfaces connected to these pins needs a pull up resistor, for instance (WE# of the NAND Flash (LFALE)) and I need to input a 0 to the config pin of the processor for a particular configuration, how can I achieve this (without an FPGA or a CPLD) as I cannot connect a pull up and a pull down on the same pin/connection.

Kindly help me in this regard,

Tags (1)
0 Kudos
Reply
1 Reply

562 Views
lunminliang
NXP Employee
NXP Employee
0 Kudos
Reply