Hi ,
We are working on P1021 customized board. We tested with NAND flash and we observed P1021 Processor is booted successfully. Now when we tried with NOR flash we were able to load images into NOR flash by using Ethernet communication port. After Loading the images P1021 is not able boot from the NOR flash. Boot Configuration for NOR flash is set to cfg_rom_loc[0:3] : 1110.
Here are following queries.
1.Is it mandatory to write Boot_sequencer to boot P1021 processor from NOR as we didn't write the boot_sequencer for NAND flash booting. If yes how the Boot_sequencer is written for NOR.
2.What are the conditions need to check and any other Init process is required while NOR booting.
Can anyone share the P1021 NOR booting sequence.
Regards,
Brahmam.
+91-9949105191
Hello brahmam yelagaturi,
Boot_sequencer for P1021 is not mandatory.
P1021 local bus signals are multiplexed with some QE funtions(eg. TDM).
You could boot from GPCM as the pins configuring eLBC signals by default, if you want to use them simultaneously, you need to use isolation logic on the board switch between QE and eLBC, please refer to P1021RDB design.
Hope the above is helpful and related with your current design.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello brahmam yelagaturi,
Please submit a service request to require P1021RDB hardware design documents from hardware team.
In addition, how did you build NOR u-boot?
Which version Linux SDK did you use?
Did you customize u-boot source based on P1021RDB or P1021MDS? Since P1021MDS doesn't support boot from NOR Flash.
Thanks,
Yiping
Hi Yiping,
Thanks for your reply.
We've designed our own P1021 customized board for Industrial Automation.After few trails we've succeeded with NOR flash loading and booting through ETSEC-1 of P1021.
We are not using any OS Kind of environments here. We've written bare-board drivers. But we're getting some issues in Etsec-2,Etsec-3(serdes) init process.
Is there any difference in ETSEC-2 and ETSEC-3(SERDES mode) controllers init process when it compared to ETSEC-1(RGMII mode).
Could you please verify the below Ethernet-2,3 init process for SERDES.
instance=etsec-2,etsec-3
#define ECNTRL_FIFM 0x00008000
#define ECNTRL_CLRCNT 0x00004000
#define ECNTRL_AUTOZ 0x00002000
#define ECNTRL_STEN 0x00001000
#define ECNTRL_GMIIM 0x00000040
#define ECNTRL_TBIM 0x00000020
#define ECNTRL_RPM 0x00000010
#define ECNTRL_R100M 0x00000008
#define ECNTRL_RMM 0X00000004
#define ECNTRL_SGMIIM 0x00000002
// initialize ethernet control register
p1021EtsecMemMap[instance].ecntrl = ECNTRL_STEN | ECNTRL_CLRCNT | ECNTRL_AUTOZ | ECNTRL_RPM | ECNTRL_SGMIIM;
// initialize station address
p1021EtsecMemMap[instance].macstnaddr1 =
((DWORD)etsec->config.macAddress[ETSEC_MAC_ADDR_OCTET_6] << SHIFT_3_BYTES) |
((DWORD)etsec->config.macAddress[ETSEC_MAC_ADDR_OCTET_5] << SHIFT_2_BYTES) |
((DWORD)etsec->config.macAddress[ETSEC_MAC_ADDR_OCTET_4] << SHIFT_1_BYTES) |
(DWORD)etsec->config.macAddress[ETSEC_MAC_ADDR_OCTET_3];
p1021EtsecMemMap[instance].macstnaddr2 =
((DWORD)etsec->config.macAddress[ETSEC_MAC_ADDR_OCTET_2] << SHIFT_3_BYTES) |
((DWORD)etsec->config.macAddress[ETSEC_MAC_ADDR_OCTET_1] << SHIFT_2_BYTES);
// initialize receive control register
p1021EtsecMemMap[instance].rctrl = 0 ;
// initialize maximum receive buffer length register
p1021EtsecMemMap[instance].mrblr = ETSEC_BUFFER_LENGTH;
// initialize DMA control register
p1021EtsecMemMap[instance].dmactrl = DMACTRL_TDSEN | DMACTRL_TBDSEN;
// initialize attribute register
p1021EtsecMemMap[instance].attr = ATTR_RDSEN | ATTR_RBDSEN;
// setup RX ring BD
etsecInitRxRing( instance, etsec->config.useInterrupts);
// setup TX ring BD
etsecInitTxRing( instance, etsec->config.useInterrupts);
// clear all interrupt, transmit, and receive events
p1021EtsecMemMap[instance].ievent = IEVENT_CLR_ALL_EVENTS;
p1021EtsecMemMap[instance].tstat = TSTAT_CLR_ALL_EVENTS;
p1021EtsecMemMap[instance].rstat = RSTAT_CLR_ALL_EVENTS;
// initialize the interrupt mask based on whether or not interrupts are being used
{
const DWORD IMASK[NUM_BOOLEANS] = {0, IMASK_ALL_EVENTS};
const BOOLEAN USE_INTERRUPTS = min( etsec->config.useInterrupts, TRUE);
p1021EtsecMemMap[instance].imask = IMASK[USE_INTERRUPTS];
}
// initialize the MAC config1 based on diagnostic type
{
const DWORD CFG1_LOOPBACK[NUM_BOOLEANS] = {0, MACCFG1_LOOPBACK};
const BOOLEAN LOOPBACK = (BOOLEAN)(etsec->config.diagType == ETSEC_DT_MAC_INTERNAL_LOOPBACK);
p1021EtsecMemMap[instance].maccfg1 = MACCFG1_RX_EN | MACCFG1_TX_EN | CFG1_LOOPBACK[LOOPBACK];
}
// set the PHY mode link type in the status
etsecDeterminePhyModeLinkType( etsec);
// set the BD and buffer addresses in the ETSEC descriptor
etsec->status.txBds = (BD8_TSEC_T *)&etsecTxBd[instance];
etsec->status.rxBds = (BD8_TSEC_T *)&etsecRxBd[instance];
etsec->status.txBufs = etsecTxBuffer[instance][0];
etsec->status.rxBufs = etsecRxBuffer[instance][0];
Regards,
Brahmam.
Hello brahmam yelagaturi,
For Non OS project design, you could refer to NetComm Software 4.4, which could be downloaded from NetComm Software Resources|Freescale.
Please refer to ETSEC_Init function in the attachment to do SGMII and RGMII initialization.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------