Hello, I'm trying to run an HelloWorld application on T2080RDB target.
I used the following instructions to setup eclipse on host PC:
Yocto Application Development Using Eclipse IDE
After compiled I transfer the binary to target by means of a usb pendrive.
When I try to run it I have the following lines:
-sh: .: ./HelloWorld: cannot execute binary file
Any suggestions about this? What's getting wrong?
解決済! 解決策の投稿を見る。
Test your board using static library for your software.
Use similar command for gcc:
$CC test.c --static -o test.elf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Test your board using static library for your software.
Use similar command for gcc:
$CC test.c --static -o test.elf
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Problem solved. I copied the file under root and changed permissions to 777.
It works.
B.R.
Hello,
thanks for the reply.
On host PC I compiled with the command you suggested to use, but when trying to execute I obtain
root@t2080rdb:/run/media/sda1# ./Hello.elf
-sh: ./Hello.elf: Permission denied
sudo command doesn't work on T2080rdb.
Which is the cause of such behavior?