I am working on a T4240QDs board. When I boot into the system, the eth0 is not generated.
I checked the dmesg dump and found out the following error messages
[ | 1.751442] fsl_mac: mac.c:417:mac_load() fsl_mac: FSL FMan MAC API based driver () |
[ | 1.758122] fsl_mac ffe4e0000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@e0000) failed |
[ | 1.766663] fsl_mac: probe of ffe4e0000.ethernet failed with error -22 |
[ | 1.771981] fsl_mac ffe4e8000.ethernet: of_get_mac_address(/soc@ffe000000/fman@400000/ethernet@e8000) failed |
[ | 1.780518] fsl_mac: probe of ffe4e8000.ethernet failed with error -22 |
[ | 1.785914] fsl_mac ffe5e8000.ethernet: of_get_mac_address(/soc@ffe000000/fman@500000/ethernet@e8000) failed |
[ | 1.794452] fsl_mac: probe of ffe5e8000.ethernet failed with error -22 |
[ | 1.799911] fsl_dpa: dpaa_eth.c:4304:dpa_load() fsl_dpa: FSL DPAA Ethernet driver () |
[ | 1.806813] fsl_dpa ethernet.16: dev_get_drvdata(ffe4e8000.ethernet) failed |
[ | 1.812483] fsl_dpa: probe of ethernet.16 failed with error -22 |
[ | 1.817219] fsl_dpa ethernet.17: dev_get_drvdata(ffe5e8000.ethernet) failed |
[ | 1.822888] fsl_dpa: probe of ethernet.17 failed with error -22 |
I booted into the U-boot prompt and tried to set the IP address
I set a suitable IP address(10.116.65.38) netmask(255.255.255.0) gatewayip(10.116.65.1)
The error that I got was:
*** ERROR: `eth1addr' not set
FM1@DTSEC5 Waiting for PHY auto negotiation to complete......... TIMEOUT !
FM1@DTSEC5: No link.
ping failed; host 10.116.65.38 is not alive
I checked the board infor structure:
=> bdinfo
memstart = 0x00000000
memsize = 0x200000000
flashstart = 0xE0000000
flashsize = 0x08000000
flashoffset = 0x00000000
sramstart = 0x00000000
sramsize = 0x00000000
immr_base = 0xFE000000
bootflags = 0x00000000
intfreq = 1666.667 MHz
busfreq = 666.667 MHz
addressing = 36-bit
ethaddr = (not set)
IP addr = 10.116.65.32
baudrate = 115200 bps
relocaddr = 0x7FF30000
Core voltage= 1043 mV
XVDD = 1.50 V
SYSCLK = 66.67 MHz
DDRCLK = 66.67 MHz
RCW source = I2C extended addressing
HRESET_REQ = Reset system
Clearly ethaddr was not set.
I am trying to figure out a way to recover the MAC address and I am not able to. Where and how do I retrieve my MAC address.
Thanks in advance.
I have attached my environment variables:
baudrate=115200
bdev=sda3
bootargs=root=/dev/mmcblk0p1 rw rootdelay=5 console=ttyS0,115200
bootcmd=setenv bootargs root=/dev/mmcblk0p1 rw rootdelay=5 console=$consoledev,$baudrate;mmcinfo;ext2load mmc 0:1 $loadaddr $bootfile;ext2load mmc 0:1 $fdtaddr $fdtfile; bootm $loadaddr - $fdtaddr
bootdelay=10
bootfile=uImage
c=ffe
consoledev=ttyS0
ethact=FM1@DTSEC5
ethprime=FM1@DTSEC1
fdtaddr=0x17200000
fdtfile=uImage-t4240qds.dtb
filesize=0x3df080
fman_ucode=0xeff40000
gatewayip=10.116.65.1
hwconfig=fsl_ddr:ctlr_intlv=3way_4KB,bank_intlv=auto;usb1:dr_mode=host,phy_type=utmi
ipaddr=10.116.65.32
loadaddr=0x10000000
netdev=eth0
netmask=255.255.255.0
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate $othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp $fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=0x02000000
ramdiskfile=t4240qds/ramdisk.uboot
rootpath=/opt/nfsroot
serverip=10.116.65.38
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize && erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize && protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize
uboot="u-boot.bin"
ubootaddr=0xeff80000
解決済! 解決策の投稿を見る。
Hello,
This is the solution to the issue that I have raised. And this issue is currently resolved.
The FMAN u code (version 106.4.6) is the issue. I updated the FMAN ucode from the version that arrived in the board (106.4.6) to 106.4.9
Version 106.4.9+ would work on the board and I was able ping my network.
The SDK documentation had the method to perform this:
The NOR flash on the DPAA board has two flash banks
Bank switching can be done in U-Boot using the following statements:
• Switch to bank 0: reset
• Switch to alternate bank: qix altbank
Programming a new ucode
0xebf40000 is the location of ucode in the alternate bank.
=>tftp 1000000 <ucode_file_name>.bin
=>erase ebf40000 ebf5ffff
=>cp.b 1000000 ebf40000 $filesize
=>qix altbank
Is FMAN microcode uploaded in u-boot?
Would you please also share your u-boot setup log?
Thank you for the reply!! My U-boot log is:
U-Boot 2013.01 (Jun 12 2013 - 16:13:31), Build: jenkins-york-fsl-u-boot-119
CPU0: T4240E, Version: 1.0, (0x82480010)
Core: E6500, Version: 1.0, (0x80400010)
Clock Configuration:
CPU0:1666.667 MHz, CPU1:1666.667 MHz, CPU2:1666.667 MHz, CPU3:1666.667 MHz,
CPU4:1666.667 MHz, CPU5:1666.667 MHz, CPU6:1666.667 MHz, CPU7:1666.667 MHz,
CPU8:1666.667 MHz, CPU9:1666.667 MHz, CPU10:1666.667 MHz, CPU11:1666.667 MHz,
CCB:666.667 MHz,
DDR:800 MHz (1600 MT/s data rate) (Asynchronous), IFC:166.667 MHz
FMAN1: 444.444 MHz
FMAN2: 333.333 MHz
QMAN: 333.333 MHz
PME: 333.333 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 14180019 0c101914 00000000 00000000
00000010: 04383063 30548c00 1c020000 1d000000
00000020: 00000000 ee0000ee 00000000 000307fc
00000030: 00000000 00000000 00000000 00000020
Board: T4240QDS, Sys ID: 0x1e, Sys Ver: 0x24, vBank: 0
FPGA: v3 (T4240QDS_2012_1113_1114), build 438 on Tue Nov 13 17:14:23 2012
SERDES Reference Clocks: SERDES1=125MHz SERDES2=125MHz SERDES3=100MHz SERDES4=100MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM 9JSF25672AZ-2G1K1
Detected UDIMM 9JSF25672AZ-2G1K1
Detected UDIMM 18KSF51272AZ-1G6K1
Not all DIMMs are identical. Memory controller interleaving disabled.
6 GiB left unmapped
DDR: 8 GiB (DDR3, 64-bit, CL=11, ECC on)
Flash: 128 MiB
L2: 2048 KB enabled
enable l2 for cluster 1 fec60000
enable l2 for cluster 2 feca0000
Corenet Platform Cache: 1536 KB enabled
Using SERDES1 Protocol: 1 (0x1)
Using SERDES2 Protocol: 28 (0x1c)
Using SERDES3 Protocol: 6 (0x6)
Using SERDES4 Protocol: 12 (0xc)
SRIO1: enabled
SRIO2: disabled
NAND: 512 MiB
MMC: FSL_SDHC: 0
EEPROM: CRC mismatch (752b828e != db2d5536)
PCIe1: Root Complex, no link, regs @ 0xfe240000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, no link, regs @ 0xfe260000
PCIe3: Bus 01 - 01
PCIe4: disabled
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.4.6
Fman2: Uploading microcode version 106.4.6
FM1@DTSEC5, FM2@DTSEC5
You need to configure MAC addresses in u-boot environment, otherwise Kernel will report errors which you encountered, please refer to the following configuration from T4240 demo board.
eth10addr=00:e0:0c:00:ae:0a
eth11addr=00:e0:0c:00:ae:0b
eth12addr=00:e0:0c:00:ae:0c
eth13addr=00:e0:0c:00:ae:0d
eth14addr=00:e0:0c:00:ae:0e
eth15addr=00:e0:0c:00:ae:0f
eth1addr=00:e0:0c:00:ae:01
eth2addr=00:e0:0c:00:ae:02
eth3addr=00:e0:0c:00:ae:03
eth4addr=00:e0:0c:00:ae:04
eth5addr=00:e0:0c:00:ae:05
eth6addr=00:e0:0c:00:ae:06
eth7addr=00:e0:0c:00:ae:07
eth8addr=00:e0:0c:00:ae:08
eth9addr=00:e0:0c:00:ae:09
ethact=e1000#0
ethaddr=00:e0:0c:00:ae:00
Thank you! It worked perfectly.
And further when I boot the board and set the Ip address using:
ifconfig fm2-mac5 inet 10.116.65.8 netmask 255.255.255.0
and set the default gateway with:
route add default gw 10.116.65.1
I am not able to ping a machine with IP 10.116.65.38 in the same network.
Thanks in advance.
EDIT: I had raised the question of why the board had 16 variables, I checked the T4240 manual and figured that it has 16, 1Gbps Ethernet MACs. Thanks.
Please check whether you could ping gateway successfully,
The dtb file also defines 16 Ethernet MACs, probably they are not enabled simultaneously, this is decided by RCW.
I am not able to ping the default gateway. We suspect it's IP tunneling, should we consider that to be the issue?
Please check whether you could use FM2@DTSEC5 in u-boot.
=> setenv ethact FM2@DTSEC5
=>setenv ipaddr 10.116.65.8
=>ping 10.116.65.38
In Linux, please try to use "ethtool" to check the ethernet port status.
Please check your network environment with your PC.
Thank you!! I have tried out various methods to mitigate this error, and still the ping utility within the kernel is not able to find my host machine.
Within u-boot when I ping my host machine, the prompt ends with:
Using FM2@DTSEC5 device
host 10.116.65.38 is alive
In addition I have been able to download a kernel from my host machine and boot it, using tftp.
and ethact IS set to:
=> printenv ethact
ethact=FM2@DTSEC5
However when I set an IP to fm2-mac5 interface the network doesnt seem to be reachable.
Here is the ouput of my ifconfig
root@t4240qds:~# ifconfig fm2-mac5
fm2-mac5 Link encap:Ethernet HWaddr 00:04:9f:02:e5:a7
inet addr:10.116.65.8 Bcast:10.116.65.255 Mask:255.255.255.0
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe5e8000-fe5e8fff
And my IP table, before and after adding the default IP:
root@t4240qds:~# route
Kernel IP routing table
Destination Gateway Genmask Flags Metric Ref Use Iface
10.116.65.0 * 255.255.255.0 U 0 0 0 fm2-mac5
root@t4240qds:~# route add default gw 10.116.65.1
root@t4240qds:~# route
Kernel IP routing table
Destination Gateway Genmask Flags Metric Ref Use Iface
default 10.116.65.1 0.0.0.0 UG 0 0 0 fm2-mac5
10.116.65.0 * 255.255.255.0 U 0 0 0 fm2-mac5
And the ping output:
root@t4240qds:~# ping 10.116.65.1
PING 10.116.65.1 (10.116.65.1): 56 data bytes
64 bytes from 10.116.65.8: Destination Host Unreachable
Vr HL TOS Len ID Flg off TTL Pro cks Src Dst Data
4 5 00 0054 0000 2 0000 40 01 a3b8 10.116.65.8 10.116.65.1
64 bytes from 10.116.65.8: Destination Host Unreachable
We have an additional T4240 board and with the same configuration this seems to be the issue in both the boards. Is there anything I am missing? Or is any of these methods wrong?
(As far as the netowrk is concerned, I attached the ethernet to another machine and was able to ping my host, with the same IP configuration)
I checked the Quick Start Guide, and in the bot log, once udevd was started, udeved proceeded to rename interface eth3 till eth7.. No such log was found in the my bootlog..
Did you use Kernel and dtb images from the the pre-built image ISO?
Would you please attach your Kernel boot log?
I am using a kernel built from the qoriq sdk framework. I also tried this on the kernel that is there in the NOR flash image that shipped with the system. Nevertheless the problem persisted in both the kernels.
I am attaching the bootlog of both these kernels
This log is the kernel from the yocto build:
T4240QDS Yocto kernel Bootlog - Pastebin.com
This log is from the kernel in the NOR flash, that arrived with the system
U-Boot 2013.01 (Jun 12 2013 - 16:13:31), Build: jenkins-york-fsl-u-boot-119 C - Pastebin.com
Thanks
No problem in the Kernel log, what is the status of ethtool.
#ifcofig fm2-mac5 10.116.65.8
#ping 10.116.65.38
#ethtool fm2-mac5
root@t4240qds:~# ifconfig fm2-mac5 10.116.65.8 netmask 255.255.255.0
root@t4240qds:~# ifconfig fm2-mac5 up
root@t4240qds:~# route add default gw 10.116.65.1
root@t4240qds:~# route
Kernel IP routing table
Destination Gateway Genmask Flags Metric Ref Use Iface
default 10.116.65.1 0.0.0.0 UG 0 0 0 fm2-mac5
10.116.65.0 * 255.255.255.0 U 0 0 0 fm2-mac5
root@t4240qds:~# ping 10.116.65.38
PING 10.116.65.38 (10.116.65.38): 56 data bytes
64 bytes from 10.116.65.8: Destination Host Unreachable
Vr HL TOS Len ID Flg off TTL Pro cks Src Dst Data
4 5 00 0054 0000 2 0000 40 01 a393 10.116.65.8 10.116.65.38
64 bytes from 10.116.65.8: Destination Host Unreachable
root@t4240qds:~# ping 10.116.65.1
PING 10.116.65.1 (10.116.65.1): 56 data bytes
64 bytes from 10.116.65.8: Destination Host Unreachable
Vr HL TOS Len ID Flg off TTL Pro cks Src Dst Data
4 5 00 0054 0000 2 0000 40 01 a3b8 10.116.65.8 10.116.65.1
Ethtool interface:
root@t4240qds:~# ethtool fm2-mac5
Settings for fm2-mac5:
Supported ports: [ MII ]
Supported link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Supported pause frame use: No
Supports auto-negotiation: Yes
Advertised link modes: 10baseT/Half 10baseT/Full
100baseT/Half 100baseT/Full
1000baseT/Full
Advertised pause frame use: No
Advertised auto-negotiation: Yes
Speed: 1000Mb/s
Duplex: Full
Port: MII
PHYAD: 1
Transceiver: external
Auto-negotiation: on
Current message level: 0xffffffff (-1)
drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol 0xffff8000
Link detected: yes
root@t4240qds:~#
Please try whether this u-boot parameter would be helpful
hwconfig=fsl_ddr:ctlr_intlv=3way_4KB,bank_intlv=auto;fsl_fm1_xaui_phy:xfi;fsl_fm2_xaui_phy:xfi;usb1:dr_mode=host,phy_type=utmi
Thank you.
I verified the Documentation and the dts file. The two 1Gbps interfaces on the board are of PHY type: RGMII
The above setting didnt make a difference and didn't work.
Can I modify it to:
fsl_ddr:ctlr_intlv=3way_4KB,bank_intlv=auto;fsl_fm1_xaui_phy:rgmii;fsl_fm2_xaui_phy:rgmii;usb1:dr_mode=host,phy_type=utmi
and test it out?
I have also attached the DTS file and the USDPAA dts file, I use. Just to make sure everything is in place.
DTS file
http://git.freescale.com/git/cgit.cgi/ppc/sdk/linux.git/tree/arch/powerpc/boot/dts/t4240qds.dts
USDPAA DTS file
sdk/linux.git - Freescale PowerPC Linux Tree
Thanks
Hi,
From the u-boot prompt I am able to ping my host machine, but my host machine is not able to ping my board. And further the RX bytes, once the kernel is loaded is always 0 and don't seem to be accepting any packets. I enabled the CONFIG_FSL_DPAA_ETH_DEBUGFS variable within the kernel and I found no hardware errors. I did check the MAC's set in the uboot environment and everything seems fine. Is there any issues in the RCW that I need to change?
I think you should have SDK image ISO QorIQ-SDK-V1.4-PPCE6500-IMAGE-20130625-yocto.iso.
Please try to use Kernel image, dtb file and filesystem in t4240qds folder like the following.
uImage-t4240qds.bin
uImage-t4240qds.dtb
fsl-image-core-t4240qds.ext2.gz.u-boot
I tried pinging the IP while performing a tftp and I was able to ping the board.
I also tried booting the machine with the pre-built images that was in the SDK. The uImage-t4240qds.bin, uImage-t4240qds.dtb and ram filesystem, fsl-image-core-t4240qds.ext2.gz.u-boot. The network still didnt respond.
I analysed the dts file
sdk/linux.git - Freescale PowerPC Linux Tree
I found that 4 MDIO slots were disabled t4240mdio2:mdio@20, mdio@40. mdio@60, mdio@80 and also the fman_oh2, fman_ph3, ... , fman1_oh6 options were also set to the status disabled.
I went ahead and removed the disable statement. The resulting kernel had a series of mdio errors and the network still didn't work out.
mdio_bus ffe5fc000: MDIO read error
mdio_bus ffe5fc000: MDIO read error
mdio_bus ffe5fc000: MDIO read error
mdio_bus ffe5fc000: MDIO read error
mdio_bus ffe5fc000: MDIO read error
mdio_bus ffe5fc000: MDIO read error
mdio_bus ffe5fc000: MDIO read error
Is the dts faulty?
Hello,
This is the solution to the issue that I have raised. And this issue is currently resolved.
The FMAN u code (version 106.4.6) is the issue. I updated the FMAN ucode from the version that arrived in the board (106.4.6) to 106.4.9
Version 106.4.9+ would work on the board and I was able ping my network.
The SDK documentation had the method to perform this:
The NOR flash on the DPAA board has two flash banks
Bank switching can be done in U-Boot using the following statements:
• Switch to bank 0: reset
• Switch to alternate bank: qix altbank
Programming a new ucode
0xebf40000 is the location of ucode in the alternate bank.
=>tftp 1000000 <ucode_file_name>.bin
=>erase ebf40000 ebf5ffff
=>cp.b 1000000 ebf40000 $filesize
=>qix altbank
You cannot ping U-Boot unless U-Boot is at the same trying to do a network operation.
If you want to check if U-Boot can be ping’ed, start, e.g., a dummy tftp that will take a while to time out with an error. While tftp is hoping for a response, you can ping U-Boot. If you can ping the external world though, then the other way will work, too.
Note that success in U-Boot means that all physical elements are ok. If, e.g., Linux fails then, you have an issue in the configuration of the device tree or driver.