It is required kvm-qemu to be available on a linux OS running on the T1040 RDB. So a fsl-image-virt image was created following SDK Technical Documentation. We deploy the image using the following commands:
=>tftp 1000000 < uImage_name>
=>tftp 2000000 fsl-image-core-<platform>.ext2.gz.u-boot
=>tftp c00000 <platform_dtb_name>
=>bootm 1000000 2000000 c00000
And we get the following errors:
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) on device 1:0.
devtmpfs: mounted
Freeing unused kernel memory: 284K (c0871000 - c08b8000)
EXT2-fs (ram0): error: ext2_check_page: bad entry in directory #3889: : rec_len is smaller than minimal - offset=0, inode=0, rec_len=0, name_len=0
EXT2-fs (ram0): error: ext2_check_page: bad entry in directory #3734: : rec_len is smaller than minimal - offset=0, inode=0, rec_len=0, name_len=0
Kernel panic - not syncing: No init found. Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.
CPU: 2 PID: 1 Comm: swapper/0 Not tainted 3.12.19-rt30-QorIQ-SDK-V1.7+g6619b8b #1
Call Trace:
[e7083e80] [c0006f50] show_stack+0x40/0x150 (unreliable)
[e7083ec0] [c06a186c] dump_stack+0x78/0xa0
[e7083ed0] [c069fbac] panic+0xd8/0x1fc
[e7083f20] [c000295c] kernel_init+0x16c/0x170
[e7083f40] [c000fe0c] ret_from_kernel_thread+0x5c/0x64
Rebooting in 180 seconds..
How can we solve this?
Thanks in advance.
解決済! 解決策の投稿を見る。
Hello Juan Rodrigo,
Please download the filesystem at 4000000.
Please refer to the following definition in include/configs/T104xRDB.h, the command line is allocated backward from 64M, if the ramdiskaddr starts at 32M, fsl-image-virt rootfs image is larger than 32M(about 44M), the command line data will be written in the middle of it, which causes the rootfs filesystem corrupted, so you will get filesystem setting up error.
/*
* For booting Linux, the board info and command line data
* have to be in the first 64 MB of memory, since this is
* the maximum mapped by the Linux kernel during initialization.
*/
#define CONFIG_SYS_BOOTMAPSZ (64 << 20) /* Initial map for Linux*/
#define CONFIG_SYS_BOOTM_LEN (64 << 20) /* Increase max gunzip size *
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Juan Rodrigo,
Please download the filesystem at 4000000.
Please refer to the following definition in include/configs/T104xRDB.h, the command line is allocated backward from 64M, if the ramdiskaddr starts at 32M, fsl-image-virt rootfs image is larger than 32M(about 44M), the command line data will be written in the middle of it, which causes the rootfs filesystem corrupted, so you will get filesystem setting up error.
/*
* For booting Linux, the board info and command line data
* have to be in the first 64 MB of memory, since this is
* the maximum mapped by the Linux kernel during initialization.
*/
#define CONFIG_SYS_BOOTMAPSZ (64 << 20) /* Initial map for Linux*/
#define CONFIG_SYS_BOOTM_LEN (64 << 20) /* Increase max gunzip size *
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Yiping.
Thank you for your answer. I followed your suggestions and everything went OK.
Juan.