I am compiling the u-boot with standalone toolchain installed in /opt/fsl-qoriq/2.0
to use the toolchain, I source the /opt/fsl-qoriq/2.0/environment-setup-ppc64e5500-fsl-linux. Its OK since I verified by compiling a simple C program.
But when compiling u-boot I get the error:
powerpc64-fsl-linux-ld.bfd: skipping incompatible /opt/fsl-qoriq/2.0/sysroots/ppc64e5500-fsl-linux/usr/lib64/powerpc64-fsl-linux/4.9.2/libgcc.a when searching for -lgcc
powerpc64-fsl-linux-ld.bfd: cannot find -lgcc
Screenshot attached. SDK version: QorIQ Linux SDK v2.0
I have the same problem when I compile the U-Boot for B4860QDS with standalone toolchain installed in /opt/fsl-qoriq/2.0. The error is:
CC examples/standalone/hello_world.o
LD examples/standalone/hello_world
powerpc64-fsl-linux-ld.bfd: skipping incompatible /opt/fsl-qoriq/2.0/sysroots/ppc64e6500-fsl-linux/usr/lib64/powerpc64-fsl-linux/4.9.2/libgcc.a when searching for -lgcc
powerpc64-fsl-linux-ld.bfd: cannot find -lgcc
make[3]: *** [examples/standalone/hello_world] error 1
And anybody can help me resolve the problem, Thanks!
Do the following:
1. Obtain the 32-bit binary disc image for e5500-based processors. The link below is the entry point to the download procedure, note there are no shortcuts:
http://www.nxp.com/products/microcontrollers-and-processors/more-processors/application-specific-mcu...
The name of the image should be something like "QorIQ Linux SDK v2.0 PPCE5500 IMAGE.iso"
2. Mount the disc and cd to fsl-toolchain/
3. Execute one of the installation scripts in that directory, whichever appropriate for your host architecture.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
From the following discussion I find that the 32-bit toolchain should be used for u-boot:
standalone compilation of u-boot for T1040 using QORIQ SDK1.7
but not sure how to install the 32-bit toolchain?
I mean how to install the toolchain from SDK iso, and not via bitbake, as mentioned there?
This file is present: "fsl-qoriq-glibc-x86_64-ppc64e5500-toolchain-2.0.sh"
but this file is not present; "fsl-qoriq-glibc-x86_64-ppce5500-toolchain-2.0.sh"