Do I have to comply with T1022's power on time sequence? If I don't comply with it and power up all the power-supply rails at the same time. What will happen? Can T1022 work normally?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do I have to comply with T1022's power on time sequence? If I don't comply with it and power up all the power-supply rails at the same time. What will happen? Can T1022 work normally?

527件の閲覧回数
hitrichard
Contributor I

Now I  am using T1022 to design a board. As shown in the datasheet page 53, it lists a power sequence. Now I want to ask that do I have to comply with T1022's power up sequence? If I don't comply with it and power up all the power-supply rails at the same time. What will happen? Can T1022 work normally?

0 件の賞賛
返信
1 返信

476件の閲覧回数
ufedor
NXP Employee
NXP Employee

Normal processor operation is not guaranteed if requirements of its Data Sheet are violated.

0 件の賞賛
返信