Demos for T1040D4RDB-PA

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Demos for T1040D4RDB-PA

1,268件の閲覧回数
walter95
Contributor I

Hi, this is my first time using nxp T1040D4RDB-PA and i'm looking for demos to help me understand how the board works.

Thank you

0 件の賞賛
返信
5 返答(返信)

1,264件の閲覧回数
bpe
NXP Employee
NXP Employee

All available software for T1040 can be found in NXP QorIQ SDK:

https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk...

Best Regards,
Platon

 

 

0 件の賞賛
返信

1,262件の閲覧回数
walter95
Contributor I

I am installing QorIQ SDKV1.8 on Ubuntu and getting following error while executing host-prepare.sh:

could not find "libbonobo2-common"

fail to install pkgs on host

0 件の賞賛
返信

1,244件の閲覧回数
bpe
NXP Employee
NXP Employee

SDK 1.8 was only tested with Ubuntu 14.04. It may fail if you attempt to install it on a later version. If you are installing on Ubuntu 14.04, and there are still error messages, check this post for more suggestions.

Hope this helps,
Platon

0 件の賞賛
返信

1,238件の閲覧回数
walter95
Contributor I

I solved it by installing ubuntu 14.04. But after I installed the SDK, where do I find some bare metal examples (i.e. without an operating system) to be tested on the board?

0 件の賞賛
返信

1,210件の閲覧回数
bpe
NXP Employee
NXP Employee

No bare board software demos are available for T1040, sorry. If you are looking for a reference code to bringup and control a peripheral, you can look at Linux drivers:

https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-08616F56-1369-47B0-B...

 

Best Regards,
Platon

0 件の賞賛
返信