DDR_SDRAM_MODE register configuration!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR_SDRAM_MODE register configuration!

2,124 Views
qammarabbas
Contributor IV

Hi,
I am trying to configure the DDR Memory Controller registers of T1042. While configuring the DDR_SDRAM_MODE register i found that that DDR_SDRAM_MODE [WR] field (bit number 20-22 of the register) should be given the same value as assigned to the field WRREC in the TIMING_CFG_1 register. The confusion here is that WRREC field in the TIMING_CFG_1 register is of 4 bits whereas the WR field in DDR_SDRAM_MODE register is of 3 bits. I want to configure it to "15 cycles" that require 4 bits. Please guide me how can i achieve that?


Please find the attached manual for information. Thank you!

Tags (1)
2 Replies

1,811 Views
ufedor
NXP Employee
NXP Employee

DDR3 SDRAM does not support Write Recovery "15 cycles":

2017-11-14_150701.jpg

1,811 Views
qammarabbas
Contributor IV

Thanks!

0 Kudos
Reply