Are there differences in ls1043 board revisions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Are there differences in ls1043 board revisions

518 次查看
brianpaiva
Contributor III

I have no LS1043ARDB boards here.  The newer one is SCH-28529 REV C1 and the older one is SCH-28529 REV C.  The differences log on the schematic for REV C1 says the only difference is setting the EVDD in the CPLD, however I am noticing strange behaviour.  I've made some software changes (still trying to narrow down which) and the REV C board hangs at startup when I initialize all 4 CPUs.  The only way I can get it work is to just initialize one.  The REC C1 board is fine in both cases.

There are other issue with the Rev C.  I have run from bank v4 because bank v0 can't run 'dhcp' successfully, and I think something is wrong with the NAND because u-boot prints out this:

Using SERDES1 Protocol: 5205 (0x1455)
Flash: 128 MiB
NAND: fsl_ifc_read_byte beyond end of buffer
fsl_ifc_read_byte beyond end of buffer
fsl_ifc_read_byte beyond end of buffer
fsl_ifc_read_byte beyond end of buffer

Is there anything not listed between the Rev C and C1 that explains this CPU problem?

0 项奖励
1 回复

344 次查看
ufedor
NXP Employee
NXP Employee

It is reasonable to investigate the issue as a Technical Case:

https://community.freescale.com/thread/381898

0 项奖励