Hello!
I have lx2160a there is onboard NI I have used by running DPDK app. and use only
dpdk-extras/dpaa2/dynamic_dpl.sh dpmac.10 dpmac.9 dpmac.8 dpmac.7 dpmac.6 dpmac.5 ...
As a result I see a number of dpni.X devices ...
Now I insert a yet another network card on board (it's MT26448 ) and just is puzzled how to make ports of the card available for DPDK ?
Is there simple procedure step-by-step to do this ?
PS:On intel I use dpdk-devbind ... but on the LX this cannot be used.
Hello!
Is there any who can me help to resolve a problem ?
This is not QEMU or any other HyperVisor related problem. I running DPDK apps on the NXP ls2160a.
Is the adding discrete NIC is supported in the NXP at all ?
Hi @SysManOne
Please refer below link to set up device using dpdk scripts.
Thanks
Khushbu
Thanks
Khushbu
Hi !
Thanks for the answer.
#./dpdk-extras/dpaa2/dynamic_dpl.sh dpmac.10 dpmac.9 dpmac.8 dpmac.7
# ${HOME}/dpdk-extras/dpaa2/dynamic_dpl.sh dpmac.10 dpmac.9 dpmac.8 dpmac.7
${HOME}/dpdk-extras/dpaa2/dynamic_dpl.sh dpmac.10 dpmac.9 dpmac.8 dpmac.7 dpmac.6 dpmac.5 dpmac.4
++ /root/dpdk-extras/dpaa2/dynamic_dpl.sh dpmac.10 dpmac.9 dpmac.8 dpmac.7 dpmac.6 dpmac.5 dpmac.4
Using board type as 2160
Using High Performance Buffers
mkdir: cannot create directory ‘/mnt/hugepages’: File exists
##################### Container dprc.2 is created ####################
Container dprc.2 have following resources :=>
* 16 DPBP
* 8 DPCON
* 8 DPSECI
* 7 DPNI
* 24 DPIO
* 2 DPCI
######################### Configured Interfaces #########################
Interface Name Endpoint Mac Address
============== ======== ==================
dpni.1 dpmac.10 00:00:00:00:0:10
dpni.2 dpmac.9 00:00:00:00:0:9
dpni.3 dpmac.8 00:00:00:00:0:8
dpni.4 dpmac.7 00:00:00:00:0:7
dpni.5 dpmac.6 00:00:00:00:0:6
dpni.6 dpmac.5 00:00:00:00:0:5
dpni.7 dpmac.4 00:00:00:00:0:4
export DPRC=dprc.2
++ export DPRC=dprc.2
++ DPRC=dprc.2
root@TTR:~/Works/tootoo2# dpdk-devbind.py -s
Network devices using kernel driver
===================================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' if=enP1p1s0,enP1p1s0d1 drv=mlx4_core unused=vfio-pci,uio_pci_generic
root@TTR:~/Works/tootoo2# dpdk-devbind.py -b uio_pci_generic 0001:01:00.0
Error: bind failed for 0001:01:00.0 - Cannot bind to driver uio_pci_generic: [Errno 19] No such device
Error: unbind failed for 0001:01:00.0 - Cannot open /sys/bus/pci/drivers//unbind: [Errno 13] Permission denied: '/sys/bus/pci/drivers//unbind'
root@TTR:~/Works/tootoo2# dpdk-devbind.py -s
Other Network devices
=====================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' unused=mlx4_core,vfio-pci,uio_pci_generic
What i did wrong ?
Hi @khushbur !
1 - root@TTR:~/Works/tootoo2# dpdk-devbind.py -s
Network devices using kernel driver
===================================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' if=enP1p1s0,enP1p1s0d1 drv=mlx4_core unused=vfio-pci,uio_pci_generic
2 - root@TTR:~/Works/tootoo2# dpdk-devbind.py -b uio_pci_generic 0001:01:00.0
Error: bind failed for 0001:01:00.0 - Cannot bind to driver uio_pci_generic: [Errno 19] No such device
Error: unbind failed for 0001:01:00.0 - Cannot open /sys/bus/pci/drivers//unbind: [Errno 13] Permission denied: '/sys/bus/pci/drivers//unbind'
3 - root@TTR:~/Works/tootoo2# dpdk-devbind.py -s
Other Network devices
=====================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' unused=mlx4_core,vfio-pci,uio_pci_generic
Hi @khushbur !
root@TTR:~# dpdk-devbind.py -s
Other Network devices
=====================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' unused=mlx4_core,vfio-pci,uio_pci_generic
root@TTR:~# dpdk-devbind.py -b none 0001:01:00.0
Notice: 0001:01:00.0 MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] is not currently managed by any driver
root@TTR:~# dpdk-devbind.py -b uio_pci_generic 0001:01:00.0
Error: bind failed for 0001:01:00.0 - Cannot bind to driver uio_pci_generic: [Errno 19] No such device
Hi @khushbur !
root@TTR:~/Works/tootoo2/build# dpdk-devbind.py -s
Other Network devices
=====================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' unused=mlx4_core,vfio-pci,uio_pci_generic
root@TTR:~/Works/tootoo2/build# dpdk-devbind.py -b none 0001:01:00.0
Notice: 0001:01:00.0 MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] is not currently managed by any driver
root@TTR:~/Works/tootoo2/build# dpdk-devbind.py -b mlx4_core 0001:01:00.0
Error: bind failed for 0001:01:00.0 - Cannot bind to driver mlx4_core: [Errno 19] No such device
root@TTR:~/Works/tootoo2/build# dpdk-devbind.py -b vfio-pci 0001:01:00.0
root@TTR:~/Works/tootoo2/build# dpdk-devbind.py -s
Network devices using DPDK-compatible driver
============================================
0001:01:00.0 'MT26448 [ConnectX EN 10GigE, PCIe 2.0 5GT/s] 6750' drv=vfio-pci unused=mlx4_core,uio_pci_generic
Hi @SysManOne
Looks like you are able to bind device to vfio-pci. Please refer below link for more details.
Thanks
Khushbu