Hi All
I am using T2080 in my application. I planned to connect MT28FW02GBBA1HPC-0AAT
nor flash(16bits 256MB) to the IFC bus. I planned to use x16 bit external latch for address/date demux application. How to interface this devices, My flash is having 27bit addressing.
I have connected like this whether this will work ?
IFC_A[16:31] -> A[15:0]
[IFC_AD[5:15] -> latch -> A[26:16]
IFC_AD[0:15] <-> DQ[15:0]
IFC_CS0# -> CE#
IFC_OE# -> OE#
IFC_WE0# -> WE#
IFC_WP0# -> WP#
IFC_RB0# -> R/B#
1.8V -> VIO
3.3V -> VCC
Regards,
Kong
From the T2080 side, each address value addresses one byte. As long as your flash is 16-bit, this means each address value in flash will address one 16-bit value (two bytes). To connect this flash, least significant address line IFC_A[31] should not be used for connection, least significant address bit, connected to flash A0 - should be IFC_A[30].
Also, flash WP# and R/B# should be pulled-up through pull-up resistors at flash side and not used for connection to IFC.
Have a great day,
Alexander
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------