在官网下载了一个iso.直接放在Linux里面解压了。

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

在官网下载了一个iso.直接放在Linux里面解压了。

936 Views
itachizheng
Contributor I

1.下载的是 

Cache: QorIQ Linux SDK v2.0 AARCH64 Yocto3.4 GBQorIQ Linux SDK v2.0 AARCH64 Yocto Cache.iso

2.使用了rar工具解压了.发现有一个install&tar.gz.  压缩文件需要运行install自动安装。生成了一个目录sstate-cache.然后就没了。

3。请问怎么生成的是android系统目录结构。

0 Kudos
Reply
2 Replies

758 Views
Pavel
NXP Employee
NXP Employee

Look at documentation for NXP SDK 2.0-1701:

http://www.nxp.com/assets/documents/data/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

This file contains information for installing and using this SDK.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

758 Views
itachizheng
Contributor I

thanks very much . let me try it .

0 Kudos
Reply