Time Sensitive Networking on LS1028ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Time Sensitive Networking on LS1028ARDB

Time Sensitive Networking on LS1028ARDB

Time Sensitive Networking(TSN) is an extension to traditional Ethernet networks, providing a set of standards compatible with IEEE 802.1 and 802.3. TSN aims to provide guarantees for deterministic latency and packet loss under congestion, allowing critical and non-critical traffic to be converged in the same network. This document introduces basic concept of Time Sensitive Networking, LS1028 TSN switch and using TSN features on LS1028ARDB.

TSN Introduction

TSN in LS1028

Using TSN features on LS1028ARDB

附件
评论

Time Sensitive Networking(TSN) is an extension to traditional Ethernet networks, providing a set of standards compatible with IEEE 802.1 and 802.3. TSN aims to provide guarantees for deterministic upsers portal latency and packet loss under congestion, allowing critical and non-critical traffic to be converged in the same network.

无评分
版本历史
最后更新:
‎09-14-2019 03:30 AM
更新人: