hello everyone:
did someone meet the following problem?
the glibc version i have used:
glibc-headers-2.5-81.el5_8.7
glibc-common-2.5-81.el5_8.7
glibc-devel-2.5-81.el5_8.7
glibc-utils-2.5-81.el5_8.7
glibc-2.5-81.el5_8.7
meet the conditions for installing ltib >2.2.x
when i input the command "./ltib -c", the question occurs:
[/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1/build-glibc/socket/sa_len.o] Error 1
make[2]: *** Waiting for unfinished jobs....
make[2]: Leaving directory `/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1/socket'
make[1]: *** [socket/subdir_lib] Error 2
make[1]: Leaving directory `/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1'
make: *** [all] Error 2
error: Bad exit status from /home/xxx/ltib-p2020rdb-20100428/tmp/rpm-tmp.86727 (%build)
RPM build errors:
Bad exit status from /home/xxx/ltib-p2020rdb-20100428/tmp/rpm-tmp.86727 (%build)
Build time for glibc-2.10: 261 seconds
Failed building glibc-2.10
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Tue Oct 9 14:16:40 2012
Ended: Tue Oct 9 14:22:14 2012
Elapsed: 334 seconds
These packages failed to build:
glibc-2.10
Build Failed
in the dir "/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1/build-glibc/socket/"
i cannot find the files of sa_len.o and subdir_lib, and sa_len.o.dt is a empty file。the normal files are coexisting with the "****.o " and "****.o.dt" formats.
help me please! i'm new in embeded linux developing
thank u very much.
isn't the key of the problem that the version of glibc for my linux os centos 5 is 2.5.81, but the glibc version of my ltib is 2.10?
if so ,how can solve it ?
it's amazing!!!!
why i change the configuring parameter of glibc to uclibc, build failed, and prompt the message "kernel-2.6.x build failed"
and then i change back to be glibc, build successed!!!
what's wrong???