Hi All,
I am using PSC9131 in my development. When I tried to run a sample bareboard project in PA, I got the following error
"CCSProtocolPlugin : CCS: Cable disconnected
[CCS last error: Cable disconnected (target power not detected) ]
"
The same env (project, USB TAP) is working for board #1. But got the above error for board #2.
--- I verified the switch settings in both the boards, it is same.
--- I checked the output from UART.
-- For Board #1, I am getting U-Boot messages, but for Board #2 nothing comes.
Please help me in resolving this.
--Hari
Hi Hari,
It looks like is a hardware issue with your board. Please check is the LED that indicate 5V and 12V are green. Also, if you still see this problem after you check the power supply for the board, you should process an RMA.
RMA is Return Merchandise Authorization (return to the factory). Please log a service request using www.freescale.com (Support -> Technical Service Request) and let me know the SR number for making it as soon as possible.
Adrian
Hi Adrian,
I checked with some other boards also and found three of them are having issues like below
Board #1: (S/N 1015)
LED D6, D7 and D9 are glowing after power ON, nothing in the console
Board #2: (S/N 52)
LED D6-D10 are glowing after power ON, nothing in the console
Board #3: (S/N
LED D6, D7, D9 and D10 are glowing after power ON. "NAND boot..." is the only thing printed in the console
We have raised a service request 1-1175918367
For that board,
Initially we are getting challenge or response box asking secure debug key. We don't know the value so we gave cancel.
Then we got the following error.
"
Error launching nandfls-core0 RAM
CCSProtocolPlugin : Failed to reset the target
[CCS last error: SAP error ]
"
--HariK
We checked that thread.
One thing we have noticed is the direction of switch SW6. In the Rev A1 boards Switch SW6 is placed in reverse direction compared to other switches. When we changed switch in that way it is started working now.
Thanks.
--HariK