Errors in SDK 1.8 Linux deployment documentation for B4860QDS board?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Errors in SDK 1.8 Linux deployment documentation for B4860QDS board?

827 次查看
klauffenburger
Contributor I

According to the Freescale Information Center document, in the section "Ramdisk Deployment from Flash" for the B4860QDS board, Step 3 "Programming Ramdisk to NOR Flash", the steps are:

     3.     Programming Ramdisk to NOR Flash

The ramdisk should be downloaded to the RAM then copied to the flash address <ramdisk_start_addr>. At the U-Boot prompt, use the following commands to program the ramdisk to flash:

=>tftp 2000000 fsl-image-core-<platform>.ext2.gz.u-boot
=>protect off <ramdisk_start_addr> +$fielsize
=>erase <ramdisk_start_addr> +$filesize
=>cp.b 2000000 <ramdisk_start_addr> $filesize
=>protect on <ramdisk_start_addr> +$filesize 

I take the address specification <ramdisk_start_addr> to be one of the Rootfs addresses 0xEF300000 (alternate bank) or 0xED300000 (current bank) listed in Table 1 of the section "Flash Bank Usage" found in the same document for the same board a few sections earlier.  According to the table, the space allocated for the image at either of these addresses is 12 MBytes.

But this is the result when I attempt to execute the above listed commands:

tftp 2000000 fsl-image-core-b4860qds-64b-20150613235020.rootfs.ext2.gz.u-boot

...

Bytes transferred = 38711773 (24eb1dd hex)

=> protect off ef300000 +$filesize

Error: end address (0xf17eb1dc) not in flash!

Bad address format

The above image is a pre-built image from the SDK 1.8 package.  The apparent problem is that the image is over 38.7 MBytes in size.

What am I doing wrong here?  Did I interpret the document wrong?  Am I trying to write the image to the wrong address, or do I have the wrong image?  Is the documentation wrong?

Also, according to the hardware documentation for the board (B4860QDSRM), there are 128 MBytes of NOR flash provided on the board.  But in the Information Center document, the NOR flash address space listed in the above referenced Table 1 spans the address range 0xEC000000 to 0xEFFFFFFF, which, if my arithmatic is correct, is 64 MBytes, not 128 MBytes.

What gives here?

I'm at a dead stop here.  Thanks for any help anyone can provide.

--ken

标签 (1)
标记 (2)
0 项奖励
1 回复

563 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Ken,

On B4860QDS only 12M is allocated for rootfs, you need to use the minimal filesystem.

fsl-image-minimal-b4860qds-64b-<date>.rootfs.ext2.gz.u-boot

The core image is too large for NOR Flash.

You could use flash-image/QorIQ_SDK_V1.8_B4860QDS_20150619_NOR_Flash.bin provided in the pre-build image ISO, which could be used to flash whole images for two flash banks.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励