Hi all,
I have tried several times, to boot bsc9132qds from SPIFlash.
I did as bellow but my images can not boot.
1. make BSC9132QDS_SPIFLASH_DDRCLK133_config
2. make
3. ../boot-format/boot_format ../boot-format/config_ddr3_1gb_9132qds_1330M.dat u-boot.bin -spi bsc9132_SPI133.bin
After that i programmed bsc9132_SPI133.bin to SPI flash, but the board can not boot up event DUT READ LED already ON.
Can anyone help me resolve this problem?
Note : I can boot normally on NAND flash (by make BSC9132QDS_NAND_DDRCLK100_config).
Thanks & Best regards.
Hi all,
Can anyone help me to boot on SPIFLASH for BSC9132QDS?
Thanks & best regards,
Hello Can Van Quyen,
If you use recent SDK, please try to use config_sram_p1010rdb.dat.
In addition, please check switch configuration to configure your target board in DDRCLK133 and SPI boot mode.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Yiping Wang,
I tried it with boot_format : sdk/boot-format.git - Freescale PowerPC SD/SPI boot tool
And change the boot location to NOR it works well.
anyway, thanks for your answers.