with power supply on/off it will boot properly but when i do reboot in the linux command prompt it will print
NAND boot... WARNING: ECC not checked in SPL, check board cfg
Error: SVR = 0x86180311 corresponds to unknown CPU type. Stopping further boot
### ERROR ### Please RESET the board ###
with power supply on / off it will print
NAND boot... WARNING: ECC not checked in SPL, check board cfg
U-Boot 2011.06.913x_WUSDK_1.6 (Feb 13 2016 - 12:03:34)
CPU0: BSC9132E, Version: 1.1, (0x86180011)
Core: E500, Version: 5.2, (0x80211152)
SVR is changing in reboot what might be the problem.
please help me out in debugging this problem.
Thanks and regards
patil m
Ensure that all notes after the BSC9132 QorIQ Qonverge Baseband Processor Data Sheet, Table 1. BSC9132 Pinout Listing are fulfilled – i.e. that neither of mentioned signals is floating.
Please provide the processor connection schematics for inspection.
hello ufedor
in the design whatever you said is taken care,
but why this svr is changing from SVR = 0x86180011 to SVR = 0x86180311 when i do the reboot.
This could be caused either by a floating pin (manufacturing defect) or by a bus hold function of an external component.