PN512发热问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN512发热问题

592 Views
puzy
Contributor I

请问一下使用PN512 读卡器装在盒子里面的时候,工作时温度达到58度,是否正常?(软件设置的发射功率为100%,读卡间隔100ms和250ms差异不大)。不正常的话是什么原因导致的,怎么改进?多谢了

Tags (1)
0 Kudos
1 Reply

557 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi  普 自勇 ,

这块芯片的工作温度在-30~85之间,你查一下下面这些VDD引脚的电流,如果在规范允许范围内就不需担心。

pastedImage_1.png

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos