I have downloaded CW 10.2 Eclipse Special Edition. I didn't see PE and device inilization on menus. Has it been removed?
Thank you for your interest. I tried it for both HCS08 and 56F82xx but PE menu is not available in IDE. Also when creating new project there is no device initilaziton selection. I have CW10.1 special editon installed also. It works properly excepting PE License error for HCS08 MCUs. What's wrong with these IDEs?
Hello,
it might be an installer problem as I have seen a similar problem on another machine.
Could you check if following folder is installed on your system (start of path depends on your installation folder):
C:\Freescale\CW MCU v10.2\MCU\ProcessorExpert
Next, could you check if you have any com.freescale.processorexpert.* plugins present in
C:\Freescale\CW MCU v10.2\eclipse\plugins
As for diagnostics: could you attach the fillowing file to this thread:
eclipse\configuration\org.eclipse.equinox.simpleconfigurator\bundles.info
And: what kind of machine are you using? Windows 7 32bit? or 64bit?
Thanks,
BK
The OS is WinXP.
I have reinstalled CW now it appears on menus. But this time when I click generate code it says "Cannot generate - no active project is selected in project panel". If I choose PE when creating project and check add main.c to project, main.c is not created. Similarly for device initialization no mcu_init.c/h file is created. And in the target cpu window it says "no cpu selected". The CW 10.2 special editon contains lots of bugs.
Hello,
Looks like either you do not have a Processor Expert project selected, or you have no Processor Expert project at all in your workspace.
Maybe have a look here:
http://mcuoneclipse.wordpress.com/2012/03/09/quickstart-for-processor-expert-in-eclipse/
Hope this helps,
BK
Here is console window output:
09.Mar.2012 14:49:42 Starting Processor Expert service
System directory = C:\Freescale\CW MCU v10.2\MCU\ProcessorExpert
User working directory = C:\Documents and Settings\All Users\Application Data\Processor Expert\CWMCU_PE5_00
Internal cache directory = C:\Documents and Settings\All Users\Application Data\Processor Expert\PECache\4fa5ce92
09.Mar.2012 14:49:47 FAILED starting Processor Expert service
09.Mar.2012 14:54:59 Could not open project L/test_PE/ProcessorExpert.pe. Processor Expert service is not initiated yet.
09.Mar.2012 14:55:58 Could not open project L/test_PE/ProcessorExpert.pe. Processor Expert service is not initiated yet.
Why does PE service fail?
Hello,
please enter service-request:
https://www.freescale.com/webapp/servicerequest.create_SR.framework
best regards
Vojtech Filip
Processor Expert Support Team