PE 'Error: Unknown type info:' KSDK 1.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PE 'Error: Unknown type info:' KSDK 1.3

550件の閲覧回数
ericnetherland
Contributor II

After updating a KDS 3.2 project from KSDK  v1.2 to v1.3, I am getting a long set of errors when Processor Expert loads.

PE v3.0.2.b151214.

They are related to fsl_usb_framework and DSPI components which have new features in 1.3. The project builds and runs but it takes a much longer time to load PE and the errors are disturbing. I can see the references to these v1.3 'types' in the PE XML file but they are all set to false and I have verified that they are unchecked in the KDS Component Inspector.

Even if I create a new project and use these components I still get these errors.

Anyone know why these are occurring and how to get them to go away?

Jun 16, 2016 9:03:58 PM Starting Processor Expert service

System directory = C:\Freescale\KDS_v3\eclipse\ProcessorExpert

Internal cache directory = C:\ProgramData\Processor Expert\PECache\763dfdd0

Processor Expert license file = not used (no license file)

Jun 16, 2016 9:03:59 PM Successfully started Processor Expert service

CDE: no license found, using Community Edition License

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_DEVICE_VBUS_DETECT

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_DEVICE_VBUS_DETECT

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_HOST_VBUS_ENABLE

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_HOST_VBUS_ENABLE

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_HOST_VBUS_OVERCURRENT

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_HOST_VBUS_OVERCURRENT

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_ID

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_ID

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_VBUS_ENABLE

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_VBUS_ENABLE

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_VBUS_VALID

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_VBUS_VALID

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_SESSION_VALID

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_SESSION_VALID

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_B_SESSION_END

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_B_SESSION_END

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_VBUS_CHARGE

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_VBUS_CHARGE

Type specification is not defined "typePinPolarity", symbol: PinPolarity_USB_OTG_VBUS_DISCHARGE

Type specification is not defined "typeSignalState", symbol: PinInitState_USB_OTG_VBUS_DISCHARGE

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_DEVICE_VBUS_DETECT from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init state"/PinInitState_USB_DEVICE_VBUS_DETECT from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_HOST_VBUS_ENABLE from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init. state"/PinInitState_USB_HOST_VBUS_ENABLE from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_HOST_VBUS_OVERCURRENT from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init state"/PinInitState_USB_HOST_VBUS_OVERCURRENT from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_ID from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init state"/PinInitState_USB_OTG_ID from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_VBUS_ENABLE from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init. state"/PinInitState_USB_OTG_VBUS_ENABLE from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_VBUS_VALID from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init state"/PinInitState_USB_OTG_VBUS_VALID from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_SESSION_VALID from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init state"/PinInitState_USB_OTG_SESSION_VALID from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_B_SESSION_END from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init state"/PinInitState_USB_OTG_B_SESSION_END from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_VBUS_CHARGE from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init. state"/PinInitState_USB_OTG_VBUS_CHARGE from component /fsl_usb_framework

Error: Unknown type info: typePinPolarity in item "Polarity"/PinPolarity_USB_OTG_VBUS_DISCHARGE from component /fsl_usb_framework

Error: Unknown type info: typeSignalState in item "Init. state"/PinInitState_USB_OTG_VBUS_DISCHARGE from component /fsl_usb_framework

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterInt item = Beans\fsl_dspi\Items\1.2.0\fsl_dspi_master_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveInt item = Beans\fsl_dspi\Items\1.2.0\fsl_dspi_slave_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsMasterDma item = Beans\fsl_dspi\Items\1.2.0\fsl_dspi_masterDma_methods.item

Cannot create new item, could not load item: symbol = SdkSpecificMethodsSlaveDma item = Beans\fsl_dspi\Items\1.2.0\fsl_dspi_slaveDma_methods.item

タグ(2)
1 返信

360件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have been able to reproduce the issue in a new project. I will ask Processor Expert development team for a solution or a

workaround for this issue.

I will keep you informed.

Best Regards,
Marek Neuzil