Hi
After reading here, asking question and get answer, I have decided to start "develop" my BSP using PE (Processor expert)
I see that I have to manually add all the componenets to the project and configure it.
Is there an already prepered complete project for this TOWER ?
(example project)
Thanks
OM
BTW: I have problems understanding the initializtion code and the jumps between assembly, low_level_init, PE_low_level_init, ..
If someone can say a few words on this too, I will be gratful.
OM
Hello,
I don't have a complete one, but one which uses the SD card on that TWR module:
mcuoneclipse/Examples/TWR-K60F120M at master · GitHub
Have a look here for background information: FatFs with Kinetis | MCU on Eclipse
You might browse there for other Kinetis example projects.
About your questions:
- the application starts from the reset vector, then initializes the stack pointer
- low_level_init (I think you mean __init_hardware()) performs the core initialization, especially clock settings.
- then it performs the zero-out of global variables, plus initializes all other variables
- then it jumps to main()
- PE_low_level_init() initializes the Processor Expert components/drivers you have loaded
I hope this helps
Hi Erich
Thanks a lot for the quick answer.
I see that I have to register to github.com in order to download your example.
Right ?
Regarding the init, to things I don't get:
1. In the start vector there is a call to __iar_program_start which looks like a function to me.
Where it is defined ?
2. After that, we jump to ?main (or __cmain)
The ?main calls to:
__low_level_init (created by PE, in cpu.c) and to __iar_data_init3 (compiler generated code ?)
Then call to user main function.
Where is ?main (or __cmain) defined ?
Thanks a lot
OM
BTW: can I get your example code in email ?
OK. (Cause I manage to download only one file at the time, not the whole project)
Regarding the init, two things I don't get.
Can you explain the folloing: (?)
1. In the start vector there is a call to __iar_program_start which looks like a function to me.
Where it is defined ?
2. After that, we jump to ?main (or __cmain)
The ?main calls to:
__low_level_init (created by PE, in cpu.c) and to __iar_data_init3 (compiler generated code ?)
Then call to user main function.
Where is ?main (or __cmain) defined ?
Thanks a lot
OM