Hello ,
KDS 3.2 , TWR-K20D72M
Configure the FlexNVM partition on PE , then use the function Cpu_SetFlexNVMPartition() to set it ,
while when debug , i check the bit of "ACCERR" is set to 1 , and also it can not finish the partiton .
i have attached the project , please help me , thank you very much !
Thank you very much !
Fan
Hello,
I have already provide answers and possible reasons of this issue. Please, see the discussion thread Return ERR_FAILED when calling Cpu_SetFlexNVMPartition() using KDS, PE and K10
You can also find a demo application for the SetFlexNVMPartition() method, see the discussion thread Reset when calling SetFlexNVMPartition() using KDS, PE and K22
Best Regards,
Marek Neuzil