MC33AR6000 Blind Zone truth table

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MC33AR6000 Blind Zone truth table

MC33AR6000 Blind Zone truth table

Blind Zone is designed a current gap when excitation start raising at very beginning.  This feature is designed for a mechanical coupling delay time when engine start.

Customer can fuse the blind zone as initiation, or config/inhibit blind zone by LIN command.

Customer can refer to the attachment truth table find the blind zone result.

 

LIN have higher priority.

when BZI(OTP)=BZI(LIN)=1, BZ output=0%

For other cases:

1. LIN mode: BZ=BZ(LIN)

2. Defult mode: BZ=BZ(OTP)

BZI(OTP) BZ(OTP) BZI(LIN) BZ(LIN) BZ output
Version A & B
0 X X 0 3%
0 X X 1 12%
1 X 0 0 3%
1 X 0 1 12%
1 X 1 0 0%
1 X 1 1 0%
version C
X X   00 0%
X X   01 3,125%
X X   10 6,25%
X X   11 12,50%
version E
X X   0 3%
X X   1 6%
No LIN
X 00 X X 0%
X 01 X X 3,250%
X 10 X X 6,00%
X 11 X X 12,00%

 

标签 (1)
附件
无评分
版本历史
最后更新:
‎08-30-2021 11:10 PM
更新人: