I am unable to connect to the MC33PT2000AF chip through SPIgen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am unable to connect to the MC33PT2000AF chip through SPIgen

618件の閲覧回数
Doublemint
Contributor II

HI,NXP engineer

When I use devPT2000 studio to create microcode and register files, and use SPIgen to write the program to PT2000, I encountered the error shown in the picture.

I have connected Drive, CLK, RESETB, and the four-wire SPI signal on the PCB board. Among them, the SPI pins are connected to pins 1, 3, 5, and 7 of the 'IO PORT' on the 'KITUSBSPIDGLEVME USB-to-SPI Interface Board'.

I really don't know why the writing failed. Is there a problem with my PCB connection, or is it a problem with my program?

The power pins on the PCB board are all connected normally, and the used parts are marked in red boxes. The same goes for the pins of the dongle. The error message from SPIgen is also attached.

If you can help me, I would be very grateful.

Doublemint

2024.03.30

ラベル(1)
0 件の賞賛
返信
0 返答(返信)