mpc8349 mitx cant erase or progrmam flash with CW

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mpc8349 mitx cant erase or progrmam flash with CW

903件の閲覧回数
alibenbrahim
Contributor I

mpc8349 mitx cant erase or progrmam flash with CW.

using EN29LV640H:

message

Error:  Getting flash ID failed 

this is the log:

: -------------------------

Using Algorithm: amd16x1.elf

======================================================================

=== Target Configuration Settings

=== Connection:   CodeWarrior USB TAP

=== Target Processor: 8349

=== Target Init File: C:\Users\ali\Desktop\MPC8349E\mpc8349e-mitx-20070221\CW Files\8349ITX_init.cfg

======================================================================

Connecting......Connected

======================================================================

=== Execute: Erase

=== Timestamp:  Mon May  4 19:28:41 2015

=== Flash Device: MX29LV640MTTC

=== Flash Organization:   4Mx16x1

=== Flash Mem Start Addr: 0xFE000000

=== Flash Mem End Addr:   0xFE7FFFFF

======================================================================

Informing other connection clients that the target is being 'clobbered'.

Loading Flash Device Driver at: 0x00000000

Flash Driver Buffer is at:  0x00001E00

Flash Driver Buffer Size is: 0x00104200

Flash Programmer:  Flash driver reports the following error(s):

Timestamp:  Mon May  4 19:28:43 2015

0 件の賞賛
返信
3 返答(返信)

734件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

Please enable "Verify target memory writes" checkbox in the Flash Programmer "Target configuration" window.

Please check again and let us know the result.

0 件の賞賛
返信

734件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Ali Benbrahim,

Why you wrote "using EN29LV640H" but in the log it shows "Flash Device: MX29LV640MTTC"?

Regards

Lunmin

0 件の賞賛
返信

734件の閲覧回数
alibenbrahim
Contributor I

Hello Lunminliang,

2 x EN29LV640H are on the board, seems  to be detected as MX29LV640MTTC !

BR

ABB

0 件の賞賛
返信