Hi,
I flashed firmware_lx2160ardb_uboot_xspiboot.img in LX2160ARDB Rev.B board with codewarrior.
After reboot, the board put the message as follows and yellow led of D19 turned on:
RCW error encountered. In order to diagnose the error temporarily change the board configuration switches to ignore the assertion of the RESET_REQ_B signal. Please refer to board reference manual in order to locate the appropriate switch that controls this behavior.
So, I turned SW1[5] to 0 and reset the baord, but the codewarrior also put the same error message and I cannot enter the flash programming menu of codewarrior.
How can I fix this problem?
And another question.
The reason I flashed the image in my board was there was no UART1 message after boot in both xspi nor flash DEV#0 and DEV#1. But there was no yellow or red led in my board at that time.
What can cause the that situtation? What point can I check?
Thanks,
JeongHwan Kim
Thank you for reply.
RESET_REQ_B (worng RCW) problem is cleared.
I'm trying to solve No UART message problem.
The cable and terminal setting is verified OK.
I tried to boot SD card instead of XSPI nor flash, but the result was same.
So, I doubt the serial module have a problem.
Could tell me default IP address of "default" 1G MAC7 or 1G MAC8 ethernet?
If CPU is alive and only serial has a problem and the ethenet port has a IP and alive,
I wish to connect to the board with ethernet.
Thanks
You wrote:
> How can I fix this problem?
Please refer to the (ARMv8_Targeting_Manual.pdf) CodeWarrior Development Studio for QorIQ LS series - ARM V8 ISA, Targeting Manual, 9.4 Board recovery in case of missing/corrupt RCW in IFC memory and use Flash Programmer to program composite firmware image "firmware_lx2160ardb_rev2_uboot_xspiboot.img" from:
https://lsdk.github.io/components.html
section LSDK IMAGES
You wrote:
> there was no UART1 message after boot
It is needed to check that UART cable is properly connected and settings of the terminal application are correct.