i.MX6 without an external POR circuit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.MX6 without an external POR circuit

321件の閲覧回数
fletcher_wang
Contributor I
How to configure the i.MX6 to operate without an external POR circuit?
0 件の賞賛
返信
3 返答(返信)

293件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

If the external POR_B signal is not used (always held high or left unconnected), the processor defaults to the internal POR function (PMU controls generation of the POR based on the power supplies). There is no need to configure it.

i.MX6ULL has a module that generates an internal POR_B signal that is logically AND'ed with any externally applied SRC_POR_B signal. The internal POR_B signal will be held low until all of the following conditions are met:

• 4ms after the external power supply VDDHIGH_IN is valid
• 1ms after the VDD_SOC_CAP supply is valid:

Best regards.

313件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Which i.MX6 are you referring for? Could you please share exact part number?

Best regards.

0 件の賞賛
返信

298件の閲覧回数
fletcher_wang
Contributor I

i.MX6ULL, MX6Y2CVM08AB

0 件の賞賛
返信