hai... how can i find ucc device in MPC8360E boars or any quicc engine supported board through linux....?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

hai... how can i find ucc device in MPC8360E boars or any quicc engine supported board through linux....?

880 Views
jayanthkumarmj
Contributor I

hai... how can i find ucc device in MPC8360E boars or any quicc engine supported board through linux....?

Tags (1)
0 Kudos
Reply
1 Reply

742 Views
genuap
NXP Employee
NXP Employee

Not sure what you're asking - are you asking how you identify them in Linux?

The UCC's are defined in the QEIWRM manual. They're in the address map, and you should be able to find them in the address map in U-boot, for example. If you're asking where they are accessed in Linux drivers I'd have to look through the source.

0 Kudos
Reply